<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックSD with freeRTOS</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SD-with-freeRTOS/m-p/1232014#M43956</link>
    <description>&lt;P&gt;Good afternoon,&lt;BR /&gt;I am using the LPC54628 test board.&lt;BR /&gt;I build my project with freeRTOS , and when creating it I add in the SDKs the SD part, because I want to save files on a card.&lt;/P&gt;&lt;P&gt;Once the project is created, without writing anything I compile it and I get an error.&lt;/P&gt;&lt;P&gt;I use MCUXPRESSO 11.3.0&lt;BR /&gt;SDK2.9.0&lt;/P&gt;&lt;P&gt;If anyone has had this happen I would appreciate your help.&lt;BR /&gt;I have tried with the examples, those with freeRTOS and those without freeRTOS, and they all compile.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 17 Feb 2021 10:40:46 GMT</pubDate>
    <dc:creator>Nadia</dc:creator>
    <dc:date>2021-02-17T10:40:46Z</dc:date>
    <item>
      <title>SD with freeRTOS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SD-with-freeRTOS/m-p/1232014#M43956</link>
      <description>&lt;P&gt;Good afternoon,&lt;BR /&gt;I am using the LPC54628 test board.&lt;BR /&gt;I build my project with freeRTOS , and when creating it I add in the SDKs the SD part, because I want to save files on a card.&lt;/P&gt;&lt;P&gt;Once the project is created, without writing anything I compile it and I get an error.&lt;/P&gt;&lt;P&gt;I use MCUXPRESSO 11.3.0&lt;BR /&gt;SDK2.9.0&lt;/P&gt;&lt;P&gt;If anyone has had this happen I would appreciate your help.&lt;BR /&gt;I have tried with the examples, those with freeRTOS and those without freeRTOS, and they all compile.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Feb 2021 10:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SD-with-freeRTOS/m-p/1232014#M43956</guid>
      <dc:creator>Nadia</dc:creator>
      <dc:date>2021-02-17T10:40:46Z</dc:date>
    </item>
    <item>
      <title>Re: SD with freeRTOS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SD-with-freeRTOS/m-p/1232059#M43958</link>
      <description>&lt;P&gt;Hello again, I think I've solved it.&lt;/P&gt;&lt;P&gt;I was getting a bug in: component -&amp;gt; osa-&amp;gt; fls_os_abstraction.h.&lt;/P&gt;&lt;P&gt;line 338: #if defined(FSL_RTOS_FREE_RTOS)&lt;/P&gt;&lt;P&gt;To solve it I go to MCU C Compiler -&amp;gt; preprocessor project properties and remove the command that says FSL_RTOS_FREE_RTOS&lt;/P&gt;&lt;P&gt;I don't know why it is created this way.&lt;/P&gt;&lt;P&gt;I hope it will help someone.&lt;BR /&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Feb 2021 12:34:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SD-with-freeRTOS/m-p/1232059#M43958</guid>
      <dc:creator>Nadia</dc:creator>
      <dc:date>2021-02-17T12:34:55Z</dc:date>
    </item>
  </channel>
</rss>