<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC54605JXXXET180 Pin compatibility in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54605JXXXET180-Pin-compatibility/m-p/1229923#M43913</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the LPC54605J256ET180 parts. I wanted to ask NXP to confirm that the LPC54605J512ET180 is a pin for pin compatible part and can be a drop in replacement. Is the only difference the increase in FLASH and RAM?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you happen to know of any of the other LPC546XXJXXXET180 parts are drop in that will also save me a lot of time from going through each pin and peripheral to confirm.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;</description>
    <pubDate>Thu, 11 Feb 2021 14:32:08 GMT</pubDate>
    <dc:creator>guitardenver</dc:creator>
    <dc:date>2021-02-11T14:32:08Z</dc:date>
    <item>
      <title>LPC54605JXXXET180 Pin compatibility</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54605JXXXET180-Pin-compatibility/m-p/1229923#M43913</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the LPC54605J256ET180 parts. I wanted to ask NXP to confirm that the LPC54605J512ET180 is a pin for pin compatible part and can be a drop in replacement. Is the only difference the increase in FLASH and RAM?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you happen to know of any of the other LPC546XXJXXXET180 parts are drop in that will also save me a lot of time from going through each pin and peripheral to confirm.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;</description>
      <pubDate>Thu, 11 Feb 2021 14:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54605JXXXET180-Pin-compatibility/m-p/1229923#M43913</guid>
      <dc:creator>guitardenver</dc:creator>
      <dc:date>2021-02-11T14:32:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54605JXXXET180 Pin compatibility</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54605JXXXET180-Pin-compatibility/m-p/1230150#M43917</link>
      <description>&lt;P&gt;Hi Matt&lt;/P&gt;
&lt;P&gt;Yes, these two parts are pin to pin compatible. The only difference is FLASH/RAM size.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;TABLE width="338"&gt;
&lt;TBODY&gt;
&lt;TR&gt;
&lt;TD width="169"&gt;　&lt;/TD&gt;
&lt;TD width="84"&gt;Flash/kB&lt;/TD&gt;
&lt;TD width="85"&gt;SRAM/kB&lt;/TD&gt;
&lt;/TR&gt;
&lt;TR&gt;
&lt;TD&gt;LPC54605J256ET180&lt;/TD&gt;
&lt;TD&gt;256&lt;/TD&gt;
&lt;TD&gt;136&lt;/TD&gt;
&lt;/TR&gt;
&lt;TR&gt;
&lt;TD&gt;LPC54605J512ET180&lt;/TD&gt;
&lt;TD&gt;512&lt;/TD&gt;
&lt;TD&gt;200&lt;/TD&gt;
&lt;/TR&gt;
&lt;/TBODY&gt;
&lt;/TABLE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Fri, 12 Feb 2021 03:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54605JXXXET180-Pin-compatibility/m-p/1230150#M43917</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-02-12T03:32:26Z</dc:date>
    </item>
  </channel>
</rss>