<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC5410x : Clock Cross-Check</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-Clock-Cross-Check/m-p/1229044#M43902</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;There is a way to monitor some clocks by using CLKOUT pin. Using this feature you can select and observe certain clocks through an external pin.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="FelipeGarcia_0-1612912119348.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136928i5DAFC84FF06A9A91/image-size/medium?v=v2&amp;amp;px=400" role="button" title="FelipeGarcia_0-1612912119348.png" alt="FelipeGarcia_0-1612912119348.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 09 Feb 2021 23:09:50 GMT</pubDate>
    <dc:creator>FelipeGarcia</dc:creator>
    <dc:date>2021-02-09T23:09:50Z</dc:date>
    <item>
      <title>LPC5410x : Clock Cross-Check</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-Clock-Cross-Check/m-p/1227871#M43882</link>
      <description>&lt;P&gt;Is there a quick (and relatively easy) way using the LPCopen libraries to cross-check the rate of an external clock with that of an internal clock (e.g. IR or RTC)? This would be part of a power-up self-test to ensure that the rate of the external clock is within tolerance (or at least that it is relatively consistent with the internal clock(s)).&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 10:11:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-Clock-Cross-Check/m-p/1227871#M43882</guid>
      <dc:creator>BTaylor</dc:creator>
      <dc:date>2021-02-08T10:11:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5410x : Clock Cross-Check</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-Clock-Cross-Check/m-p/1229044#M43902</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;There is a way to monitor some clocks by using CLKOUT pin. Using this feature you can select and observe certain clocks through an external pin.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="FelipeGarcia_0-1612912119348.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136928i5DAFC84FF06A9A91/image-size/medium?v=v2&amp;amp;px=400" role="button" title="FelipeGarcia_0-1612912119348.png" alt="FelipeGarcia_0-1612912119348.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Feb 2021 23:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-Clock-Cross-Check/m-p/1229044#M43902</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-02-09T23:09:50Z</dc:date>
    </item>
  </channel>
</rss>