<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUSB MSD external flash memory</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-MSD-external-flash-memory/m-p/1228714#M43895</link>
    <description>&lt;P&gt;Hello, i'm developing using the board&amp;nbsp;&lt;SPAN&gt;LPCXpresso55s69&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I was looking at the usb_msc_ramdisk example and i was wondering if it was possible to open an external flash memory connected to the micro through a SPI interface instead of the internal micro memory.&lt;/P&gt;&lt;P&gt;Is it possible? Cause i can't find the exact point in the example to change for switching to the external memory&lt;/P&gt;</description>
    <pubDate>Thu, 11 Feb 2021 07:29:11 GMT</pubDate>
    <dc:creator>rd1</dc:creator>
    <dc:date>2021-02-11T07:29:11Z</dc:date>
    <item>
      <title>USB MSD external flash memory</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-MSD-external-flash-memory/m-p/1228714#M43895</link>
      <description>&lt;P&gt;Hello, i'm developing using the board&amp;nbsp;&lt;SPAN&gt;LPCXpresso55s69&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I was looking at the usb_msc_ramdisk example and i was wondering if it was possible to open an external flash memory connected to the micro through a SPI interface instead of the internal micro memory.&lt;/P&gt;&lt;P&gt;Is it possible? Cause i can't find the exact point in the example to change for switching to the external memory&lt;/P&gt;</description>
      <pubDate>Thu, 11 Feb 2021 07:29:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-MSD-external-flash-memory/m-p/1228714#M43895</guid>
      <dc:creator>rd1</dc:creator>
      <dc:date>2021-02-11T07:29:11Z</dc:date>
    </item>
    <item>
      <title>Re: USB MSD external flash memory</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-MSD-external-flash-memory/m-p/1231723#M43950</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/96682"&gt;@rd1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing well!&lt;/P&gt;
&lt;P&gt;If I understand properly in your application you require to&amp;nbsp; storage from a non-volatile memory (external flash) , instead of using the SRAM of the LPC55.&lt;/P&gt;
&lt;P&gt;You could take a look at the&amp;nbsp; &lt;EM&gt;USB_DeviceMscCallback&amp;nbsp;&lt;/EM&gt; , this function handles the&amp;nbsp;&amp;nbsp;read and write events for this class.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It may also be&amp;nbsp;useful to take a look&amp;nbsp; an example like the dev_msc_sdcard_bm that&amp;nbsp; implements&amp;nbsp; an&amp;nbsp; SD memory as a reference.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Feb 2021 21:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-MSD-external-flash-memory/m-p/1231723#M43950</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2021-02-16T21:00:11Z</dc:date>
    </item>
  </channel>
</rss>