<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1769 QEICAP delay/decay in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-QEICAP-delay-decay/m-p/521749#M4385</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by paulctan on Mon Feb 27 14:08:29 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I need some help with getting velocity measurements working properly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;According to 26.6.3.11 of UM10360 Rev. 2, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;QEICAP should be a copy of QEIVEL right after the last QEITIME expiry.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a test jig hooked up with a motor running around 100rpm and an US Digital E4P encoder.&amp;nbsp; QEICAP and QEIPOS work properly, *BUT* QEICAP values are decaying instead of instantly going to 0 when I stop the motor (yes, I physically stopped the shaft after stopping the motor, but QEICAP still showed decaying values!)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there some time averaging function going on with QEICAP?&amp;nbsp; If so, are there any docs on it that I may have missed?&amp;nbsp; Also, how do I disable it?&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to find the instantaneous (well almost instantaneous) velocity, however what I'm seeing is that QEICAP almost has a 1-2 second delay after the motor has stopped.&amp;nbsp; QEIPOS stops changing instantly though!!&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to use QEICAP instead of calculating the velocity based on QEIPOS (since you have it as part of the chip), but I need help!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Paul Tan.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:52:04 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:52:04Z</dc:date>
    <item>
      <title>LPC1769 QEICAP delay/decay</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-QEICAP-delay-decay/m-p/521749#M4385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by paulctan on Mon Feb 27 14:08:29 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I need some help with getting velocity measurements working properly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;According to 26.6.3.11 of UM10360 Rev. 2, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;QEICAP should be a copy of QEIVEL right after the last QEITIME expiry.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a test jig hooked up with a motor running around 100rpm and an US Digital E4P encoder.&amp;nbsp; QEICAP and QEIPOS work properly, *BUT* QEICAP values are decaying instead of instantly going to 0 when I stop the motor (yes, I physically stopped the shaft after stopping the motor, but QEICAP still showed decaying values!)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there some time averaging function going on with QEICAP?&amp;nbsp; If so, are there any docs on it that I may have missed?&amp;nbsp; Also, how do I disable it?&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to find the instantaneous (well almost instantaneous) velocity, however what I'm seeing is that QEICAP almost has a 1-2 second delay after the motor has stopped.&amp;nbsp; QEIPOS stops changing instantly though!!&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to use QEICAP instead of calculating the velocity based on QEIPOS (since you have it as part of the chip), but I need help!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Paul Tan.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:52:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-QEICAP-delay-decay/m-p/521749#M4385</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:52:04Z</dc:date>
    </item>
  </channel>
</rss>