<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 MRKIII 2-Link Linux Drivers?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MRKIII-2-Link-Linux-Drivers/m-p/1225921#M43841</link>
    <description>&lt;P&gt;Not sure this is the right location for this question.&lt;BR /&gt;&lt;BR /&gt;Are there, or will there ever be Linux Drivers for the MRKIII 2-Link (OM6718/5)?&amp;nbsp; I know the 2-Link is a OEM'd Segger J-Link, and the Synopsys mrk3 toolchain for fully supports Linux with the exception of MRLink and 2-Link driver.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;--Jim&lt;/P&gt;</description>
    <pubDate>Thu, 04 Feb 2021 00:06:36 GMT</pubDate>
    <dc:creator>jim_obrien</dc:creator>
    <dc:date>2021-02-04T00:06:36Z</dc:date>
    <item>
      <title>MRKIII 2-Link Linux Drivers?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MRKIII-2-Link-Linux-Drivers/m-p/1225921#M43841</link>
      <description>&lt;P&gt;Not sure this is the right location for this question.&lt;BR /&gt;&lt;BR /&gt;Are there, or will there ever be Linux Drivers for the MRKIII 2-Link (OM6718/5)?&amp;nbsp; I know the 2-Link is a OEM'd Segger J-Link, and the Synopsys mrk3 toolchain for fully supports Linux with the exception of MRLink and 2-Link driver.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;--Jim&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 00:06:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MRKIII-2-Link-Linux-Drivers/m-p/1225921#M43841</guid>
      <dc:creator>jim_obrien</dc:creator>
      <dc:date>2021-02-04T00:06:36Z</dc:date>
    </item>
    <item>
      <title>Re: MRKIII 2-Link Linux Drivers?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MRKIII-2-Link-Linux-Drivers/m-p/1226251#M43845</link>
      <description>&lt;P&gt;Many toolchains/IDEs that run on Linux&amp;nbsp;support J-Link out of the box. I used e.g. Crossworks for ARM under Mint (Debain-based), supporting J-Link amongst a plethora of debug pods.&lt;/P&gt;&lt;P&gt;The MCUXpresso IDE supports J-Link as well, I have two installations (again under Mint). Debugging is in fact simpler and easier than with Win10.&lt;/P&gt;&lt;P&gt;My OM13098 has a CMSIS-DAP interface, which is also supported by both IDEs.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 08:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MRKIII-2-Link-Linux-Drivers/m-p/1226251#M43845</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-02-04T08:45:45Z</dc:date>
    </item>
    <item>
      <title>Re: MRKIII 2-Link Linux Drivers?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MRKIII-2-Link-Linux-Drivers/m-p/1242785#M44205</link>
      <description>&lt;P&gt;Hi Frank.&amp;nbsp; Thanks for responding, however it doesn't help here.&amp;nbsp; I have tried passthru for the OM6718, and ubuntu identifies it as a jlink, but it clearly isn't a standard jlink.&amp;nbsp; NXP has produced their own drivers for this particular OEM'd device, standard jlink drivers won't work.&amp;nbsp; &amp;nbsp;It's a shame too, as its the only bit missing to be able to completely work in Linux on the NCF29A1.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Mar 2021 22:56:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MRKIII-2-Link-Linux-Drivers/m-p/1242785#M44205</guid>
      <dc:creator>jim_obrien</dc:creator>
      <dc:date>2021-03-09T22:56:30Z</dc:date>
    </item>
    <item>
      <title>Re: MRKIII 2-Link Linux Drivers?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MRKIII-2-Link-Linux-Drivers/m-p/1243002#M44210</link>
      <description>&lt;P&gt;Hi Jim&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;We got the confirmation that the&amp;nbsp;MRKIII 2-link&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;software driver does not support Linux and it is not planned to do it in the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;next years.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Sorry for the inconvenience.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 07:00:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MRKIII-2-Link-Linux-Drivers/m-p/1243002#M44210</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-03-10T07:00:06Z</dc:date>
    </item>
  </channel>
</rss>