<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックSet PWM output(using CTimer) to LOW when stopped</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Set-PWM-output-using-CTimer-to-LOW-when-stopped/m-p/1224782#M43817</link>
    <description>&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;I am using LPC54606 controller with PWM using CTimer.&lt;/P&gt;&lt;P&gt;When I stop the PWM using "CTIMER_StopTimer", occasionally the PWM output still remains HIGH.&lt;/P&gt;&lt;P&gt;Is there a way I can force the PWM output to go LOW when stopped?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Hemanth&lt;/P&gt;</description>
    <pubDate>Tue, 02 Feb 2021 14:20:01 GMT</pubDate>
    <dc:creator>hemanthvasista</dc:creator>
    <dc:date>2021-02-02T14:20:01Z</dc:date>
    <item>
      <title>Set PWM output(using CTimer) to LOW when stopped</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Set-PWM-output-using-CTimer-to-LOW-when-stopped/m-p/1224782#M43817</link>
      <description>&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;I am using LPC54606 controller with PWM using CTimer.&lt;/P&gt;&lt;P&gt;When I stop the PWM using "CTIMER_StopTimer", occasionally the PWM output still remains HIGH.&lt;/P&gt;&lt;P&gt;Is there a way I can force the PWM output to go LOW when stopped?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Hemanth&lt;/P&gt;</description>
      <pubDate>Tue, 02 Feb 2021 14:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Set-PWM-output-using-CTimer-to-LOW-when-stopped/m-p/1224782#M43817</guid>
      <dc:creator>hemanthvasista</dc:creator>
      <dc:date>2021-02-02T14:20:01Z</dc:date>
    </item>
    <item>
      <title>Re: Set PWM output(using CTimer) to LOW when stopped</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Set-PWM-output-using-CTimer-to-LOW-when-stopped/m-p/1226651#M43852</link>
      <description>&lt;P&gt;Hi Hemanth,&lt;/P&gt;
&lt;P&gt;I don’t think so because PWM outputs follow certain rules as you can see in &lt;STRONG&gt;17.7.1 Rules for single edge controlled PWM outputs&lt;/STRONG&gt; section of the UM. An option is that you change alternative of the pin and manually change the output to low using GPIO.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 22:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Set-PWM-output-using-CTimer-to-LOW-when-stopped/m-p/1226651#M43852</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-02-04T22:58:23Z</dc:date>
    </item>
    <item>
      <title>Re: Set PWM output(using CTimer) to LOW when stopped</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Set-PWM-output-using-CTimer-to-LOW-when-stopped/m-p/1230681#M43928</link>
      <description>&lt;P&gt;The issue got solved when I call below APIs&lt;/P&gt;&lt;P&gt;"CTIMER_Reset" &amp;amp; "CTIMER_Deinit". After these, the pin output goes LOW.&lt;/P&gt;</description>
      <pubDate>Sat, 13 Feb 2021 03:55:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Set-PWM-output-using-CTimer-to-LOW-when-stopped/m-p/1230681#M43928</guid>
      <dc:creator>hemanthvasista</dc:creator>
      <dc:date>2021-02-13T03:55:55Z</dc:date>
    </item>
  </channel>
</rss>