<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55 On-chip ROM boot via CAN FD? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-On-chip-ROM-boot-via-CAN-FD/m-p/1223897#M43796</link>
    <description>&lt;P&gt;Hello dav,&lt;/P&gt;
&lt;P&gt;Sorry, no, we have no method to change the code in ROM.&lt;/P&gt;
&lt;P&gt;You can development a Secondary bootloader for CAN-FD.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
    <pubDate>Mon, 01 Feb 2021 08:26:38 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2021-02-01T08:26:38Z</dc:date>
    <item>
      <title>LPC55 On-chip ROM boot via CAN FD?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-On-chip-ROM-boot-via-CAN-FD/m-p/1223546#M43783</link>
      <description>&lt;P&gt;The LPC55x series has a nice built-in bootloader in ROM, but I wonder if there are any ways to achieve rom-booting via CAN bus? (CAN-FD to be specific)&lt;/P&gt;&lt;P&gt;It's not listed as a valid boot peripheral in the datasheet, but I'm thinking if we could re-configure or wire the can pins in parallel to standard UART and use a fall-back mechanism so that the "Host" can detect we're not in CAN mode, run the boot-strap process, and then switch back to CAN FD.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thoughts?&lt;/P&gt;</description>
      <pubDate>Sat, 30 Jan 2021 11:57:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-On-chip-ROM-boot-via-CAN-FD/m-p/1223546#M43783</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2021-01-30T11:57:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55 On-chip ROM boot via CAN FD?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-On-chip-ROM-boot-via-CAN-FD/m-p/1223897#M43796</link>
      <description>&lt;P&gt;Hello dav,&lt;/P&gt;
&lt;P&gt;Sorry, no, we have no method to change the code in ROM.&lt;/P&gt;
&lt;P&gt;You can development a Secondary bootloader for CAN-FD.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 08:26:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-On-chip-ROM-boot-via-CAN-FD/m-p/1223897#M43796</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-02-01T08:26:38Z</dc:date>
    </item>
  </channel>
</rss>