<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Where is the GPIO pinout for LPCXpresso55S69? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1221677#M43748</link>
    <description>&lt;P&gt;You are welcome!&lt;/P&gt;</description>
    <pubDate>Wed, 27 Jan 2021 05:55:45 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2021-01-27T05:55:45Z</dc:date>
    <item>
      <title>Where is the GPIO pinout for LPCXpresso55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1219733#M43714</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I have a question regarding the usage of GPIOs of the LPCXpresso55S69 board. I have trouble finding an explanation/a picture, which GPIO routs to which output pin. Meaning, that I found the "Pins" View in the SDK:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Bildschirmfoto 2021-01-22 um 17.27.43.png" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135592i76D9897A79BC89F9/image-size/small?v=v2&amp;amp;px=200" role="button" title="Bildschirmfoto 2021-01-22 um 17.27.43.png" alt="Bildschirmfoto 2021-01-22 um 17.27.43.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt; But how do I know where e.g. PIO0_12 is on the board? I have found those two pictures, which are not helpful at all, because they don't use the same naming. So, where do I have to put my cable on my board if I want to attach it to e.g. PIO0_12? Where do I find this information? Or am I just too stupid to understand those pictures?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Bildschirmfoto 2021-01-22 um 17.28.56.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135593i55181A1169E3596D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Bildschirmfoto 2021-01-22 um 17.28.56.png" alt="Bildschirmfoto 2021-01-22 um 17.28.56.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Bildschirmfoto 2021-01-22 um 17.29.32.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135594iF71FC832F50BC78F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Bildschirmfoto 2021-01-22 um 17.29.32.png" alt="Bildschirmfoto 2021-01-22 um 17.29.32.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would be really glad if someone could point me to the correct direction.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Ximena&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jan 2021 16:30:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1219733#M43714</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2021-01-22T16:30:35Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the GPIO pinout for LPCXpresso55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1220015#M43721</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;PIO0_12 is routed as SWDIO, but not PIO0_12 for LPCXpresso55S65 board.&lt;/P&gt;
&lt;P&gt;It's not routed to P17 or P18&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1611487902770.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135625i38A176DE7C14A32A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1611487902770.png" alt="ZhangJennie_0-1611487902770.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Have a nice day&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Sun, 24 Jan 2021 11:53:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1220015#M43721</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-01-24T11:53:29Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the GPIO pinout for LPCXpresso55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1220016#M43722</link>
      <description>&lt;P&gt;PIO0_12 was just an example, I don't really want to use it. It was just a random number!!&lt;/P&gt;&lt;P&gt;I only want to know the connection between the pins on my board and the ones in the "Pin" View in the SDK. Where do I find that?&lt;/P&gt;&lt;P&gt;I just want to get a high trigger signal at one of the GPIO pins to connect an oscilloscope. I don't care which one, just one. But I cannot find any information on how to address which pin to do so...&lt;/P&gt;</description>
      <pubDate>Sun, 24 Jan 2021 11:58:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1220016#M43722</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2021-01-24T11:58:46Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the GPIO pinout for LPCXpresso55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1220193#M43724</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;If you just want to test GPIO feature, LPCXpresso55S69 board provides P1_4, P1_6 and P1_7 for it.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The LEDs in this device are controlled by LPC55Sxx ports P1_4 (Blue), P1_6 (Red), P1_7&lt;BR /&gt;(Green) with the LEDs being illuminated when the respective LED is pulled low. Note that&lt;BR /&gt;these port lines are also connected to expansion connector P18.&lt;/P&gt;
&lt;P&gt;You can check it with SDK demo code gpio_led_output. Here is pin configuration:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1611554110358.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135643i58216ECF3DC665E6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1611554110358.png" alt="ZhangJennie_0-1611554110358.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 05:55:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1220193#M43724</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-01-25T05:55:58Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the GPIO pinout for LPCXpresso55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1220296#M43728</link>
      <description>&lt;P&gt;Hello Jun,&lt;/P&gt;&lt;P&gt;thanks for your answer. Yes, I want to test the GPIO feature, but not with the LEDs &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt; So the LEDs are blinking just fine, this works. But I cannot connect a cable to the LED. And also I don't want the LEDs to blink during the whole program.&lt;/P&gt;&lt;P&gt;So is there a GPIO that I can address in my uC-program, that routs to this P18 extension connectors that is not an LED? And if so, where can I find the exact location so I can put my cable there?&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;Ximena&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 07:28:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1220296#M43728</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2021-01-25T07:28:18Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the GPIO pinout for LPCXpresso55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1220998#M43737</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;Hi &lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179312" target="_self"&gt;Ximena&lt;/A&gt;,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;I check P18 connector, there are also other GPIO pins connected. For example&amp;nbsp; PIO1_9,&amp;nbsp;PIO1_10, PIO1_15, PIO1_18.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;some of them are defined as input buttons. but you can also config it as gpio output.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1611634313186.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135782i38484D158B7476CD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1611634313186.png" alt="ZhangJennie_0-1611634313186.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For more see demo board UM and Schematic.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jan 2021 04:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1220998#M43737</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-01-26T04:24:53Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the GPIO pinout for LPCXpresso55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1221365#M43743</link>
      <description>&lt;P&gt;Hi Jun,&lt;/P&gt;&lt;P&gt;thanks a lot!! I got it now &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt; Perfect. Always very good support here.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Ximena&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jan 2021 17:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1221365#M43743</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2021-01-26T17:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the GPIO pinout for LPCXpresso55S69?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1221677#M43748</link>
      <description>&lt;P&gt;You are welcome!&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jan 2021 05:55:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Where-is-the-GPIO-pinout-for-LPCXpresso55S69/m-p/1221677#M43748</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-01-27T05:55:45Z</dc:date>
    </item>
  </channel>
</rss>