<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC5516 ADC INPUT</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-INPUT/m-p/1220255#M43727</link>
    <description>&lt;P&gt;How many volts can the internal clamping diode of the LPC5516 clamp to? If the ADC input pin voltage is -0.4V, will it affect other MCU pins?&lt;/P&gt;&lt;P&gt;I found the following pictures from the Internet. Is the GPIO architecture of LPC5516 the same? I read that the LPC5516 manual states that the minimum analog input voltage is -0.3V. Will there be any impact if it exceeds it?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="liuweiqiang_0-1611557527348.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135652iD1AF220AC329C3BA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="liuweiqiang_0-1611557527348.png" alt="liuweiqiang_0-1611557527348.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;liuweiqiang_0-1611557527348.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 25 Jan 2021 06:53:45 GMT</pubDate>
    <dc:creator>liuweiqiang</dc:creator>
    <dc:date>2021-01-25T06:53:45Z</dc:date>
    <item>
      <title>LPC5516 ADC INPUT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-INPUT/m-p/1220255#M43727</link>
      <description>&lt;P&gt;How many volts can the internal clamping diode of the LPC5516 clamp to? If the ADC input pin voltage is -0.4V, will it affect other MCU pins?&lt;/P&gt;&lt;P&gt;I found the following pictures from the Internet. Is the GPIO architecture of LPC5516 the same? I read that the LPC5516 manual states that the minimum analog input voltage is -0.3V. Will there be any impact if it exceeds it?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="liuweiqiang_0-1611557527348.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135652iD1AF220AC329C3BA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="liuweiqiang_0-1611557527348.png" alt="liuweiqiang_0-1611557527348.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;liuweiqiang_0-1611557527348.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 06:53:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-INPUT/m-p/1220255#M43727</guid>
      <dc:creator>liuweiqiang</dc:creator>
      <dc:date>2021-01-25T06:53:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5516 ADC INPUT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-INPUT/m-p/1220380#M43730</link>
      <description>&lt;P&gt;Hi, WeiQian,&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not provide the analog channel internal architecture for the LPC55xx family.&lt;/P&gt;
&lt;P&gt;Regarding the analog channel voltage range for LPC55xx family, pls refer to the VIA specs in data sheet of LPC551x.&lt;/P&gt;
&lt;P&gt;The limiting analog ADC voltage is from -0.3V to 3.96V, the normal analog ADC voltage is from 0V to VDDA.&lt;/P&gt;
&lt;P&gt;If your ADC analog voltage is out of the range from -0.3 to 3.96V, external diodes are required to protect ADC.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1611564940561.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135673iDFAA6693449B4934/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1611564940561.png" alt="xiangjun_rong_0-1611564940561.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1611564940561.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I copy the notes here from the Data sheet.&lt;/P&gt;
&lt;P&gt;[6] An ADC input voltage above 3.6 V can be applied for a short time without leading to immediate, unrecoverable failure. Accumulated&lt;BR /&gt;exposure to elevated voltages at 4.6 V must be less than 106 s total over the lifetime of the device. Applying an elevated voltage to the&lt;BR /&gt;ADC inputs for a long time affects the reliability of the device and reduces its lifetime.&lt;BR /&gt;[7] It is recommended to connect an overvoltage protection diode between the analog input pin and the voltage supply pin.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 09:00:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-INPUT/m-p/1220380#M43730</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-01-25T09:00:29Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5516 ADC INPUT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-INPUT/m-p/1221316#M43742</link>
      <description>&lt;P&gt;Extrapolating from other vendors/MCUs, about 0.6V.&lt;/P&gt;&lt;P&gt;However, not only does exceeding the max ratings reduce the lifetime, transverse currents through the clamping diodes will affect other ADC inputs, and most probably also other peripheral units.&lt;/P&gt;&lt;P&gt;I would suggest to avoid overvoltages, using proper external protection.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jan 2021 15:19:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-INPUT/m-p/1221316#M43742</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-01-26T15:19:23Z</dc:date>
    </item>
  </channel>
</rss>