<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1549: Problem with SCT triggering ADC triggering DMA at a certain frequency</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-Problem-with-SCT-triggering-ADC-triggering-DMA-at-a/m-p/1219439#M43707</link>
    <description>&lt;P&gt;Hello Omar.&lt;/P&gt;&lt;P&gt;I thought this thread got too long down the cue, so I started a new one:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-How-to-use-the-DMA-with-the-ADC/m-p/1216661#M43624" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-How-to-use-the-DMA-with-the-ADC/m-p/1216661#M43624&lt;/A&gt;&lt;/P&gt;&lt;P&gt;with a program that gets the data in the buffer.&lt;/P&gt;&lt;P&gt;Maybe I can delete this one?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jesper&lt;/P&gt;</description>
    <pubDate>Fri, 22 Jan 2021 07:57:17 GMT</pubDate>
    <dc:creator>jespermadsen</dc:creator>
    <dc:date>2021-01-22T07:57:17Z</dc:date>
    <item>
      <title>LPC1549: Problem with SCT triggering ADC triggering DMA at a certain frequency</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-Problem-with-SCT-triggering-ADC-triggering-DMA-at-a/m-p/1211743#M43571</link>
      <description>&lt;P&gt;I found this example:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/DMA-Ping-Pong-application/ta-p/1120977" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/DMA-Ping-Pong-application/ta-p/1120977&lt;/A&gt;&lt;/P&gt;&lt;P&gt;for the LPCXpressor54114 Board and changed it to match the LPC1549 LPCXpresso™ board.&lt;/P&gt;&lt;P&gt;I get ADC results in the buffer. But there are zeros and not compleately processed data there too.&lt;/P&gt;&lt;P&gt;I'm using the SCT2_Out3 to ADC0_SEQA to DMA. I'm not sure if the ADC_SEQA is setup correctly.&lt;/P&gt;&lt;P&gt;Can someone help? The code is shown below:&lt;/P&gt;&lt;P&gt;//-------------------------------------------------------------&lt;/P&gt;&lt;P&gt;#if defined (__USE_LPCOPEN)&lt;BR /&gt;#if defined(NO_BOARD_LIB)&lt;BR /&gt;#include "chip.h"&lt;BR /&gt;#else&lt;BR /&gt;#include "board.h"&lt;BR /&gt;#endif&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;#include &amp;lt;cr_section_macros.h&amp;gt;&lt;/P&gt;&lt;P&gt;#define NUM_BUFFERS 4&lt;BR /&gt;#define DMA_TRANSFER_SIZE 8&lt;BR /&gt;#define ADC_INPUT_CHANNEL 0&lt;/P&gt;&lt;P&gt;#define SCT_PWM_RATE 10000 /* PWM frequency 10 KHz */&lt;BR /&gt;#define SCT_PWM_PIN_OUT 3 /* COUT3 Generate square wave */&lt;BR /&gt;#define SCT_PWM_OUT 3 /* Index of OUT PWM */&lt;/P&gt;&lt;P&gt;uint16_t adcOut;&lt;/P&gt;&lt;P&gt;DMA_CHDESC_T ADC_TransferDescriptors[NUM_BUFFERS] __attribute__ ((aligned(512)));&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;uint16_t CapturedData[32];&lt;/P&gt;&lt;P&gt;uint16_t DMA_Sum=0;&lt;/P&gt;&lt;P&gt;/**&lt;BR /&gt;*&lt;BR /&gt;* ADC IRQ not Used right now... Only for testing&lt;BR /&gt;*/&lt;BR /&gt;void ADC_SEQA_IRQHandler(void)&lt;BR /&gt;{&lt;BR /&gt;/* If SeqA flags is set i.e. data in global register is valid then read it */&lt;BR /&gt;Chip_ADC_ClearFlags(LPC_ADC0,0xFFFFFFFF);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;void DMA_IRQHandler(void)&lt;BR /&gt;{&lt;BR /&gt;static uint16_t DMA_Sum=0;&lt;/P&gt;&lt;P&gt;DMA_Sum++;&lt;/P&gt;&lt;P&gt;if(DMA_Sum ==8)&lt;BR /&gt;{&lt;BR /&gt;DMA_Sum=4;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/* Rrror interrupt on channel 0? */&lt;BR /&gt;if ((Chip_DMA_GetIntStatus(LPC_DMA) &amp;amp; DMA_INTSTAT_ACTIVEERRINT) != 0)&lt;BR /&gt;{&lt;BR /&gt;/* This shouldn't happen for this simple DMA example, so set the LED&lt;BR /&gt;to indicate an error occurred. This is the correct method to clear&lt;BR /&gt;an abort. */&lt;BR /&gt;Chip_DMA_DisableChannel(LPC_DMA, DMA_CH0);&lt;BR /&gt;while ((Chip_DMA_GetBusyChannels(LPC_DMA) &amp;amp; (1 &amp;lt;&amp;lt; DMA_CH0)) != 0) {}&lt;BR /&gt;Chip_DMA_AbortChannel(LPC_DMA, DMA_CH0);&lt;BR /&gt;Chip_DMA_ClearErrorIntChannel(LPC_DMA, DMA_CH0);&lt;BR /&gt;Chip_DMA_EnableChannel(LPC_DMA, DMA_CH0);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* Clear DMA interrupt for the channel */&lt;BR /&gt;Chip_DMA_ClearActiveIntAChannel(LPC_DMA, DMA_CH0);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/***&lt;BR /&gt;* ____ __ __ _&lt;BR /&gt;* | _ \| \/ | / \&lt;BR /&gt;* | | | | |\/| | / _ \&lt;BR /&gt;* | |_| | | | |/ ___ \&lt;BR /&gt;* |____/|_| |_/_/ \_\&lt;BR /&gt;* / ___| ___| |_ _ _ _ __&lt;BR /&gt;* \___ \ / _ \ __| | | | '_ \&lt;BR /&gt;* ___) | __/ |_| |_| | |_) |&lt;BR /&gt;* |____/ \___|\__|\__,_| .__/&lt;BR /&gt;* |_|&lt;BR /&gt;*/&lt;BR /&gt;void DMA_Setup(void)&lt;BR /&gt;{&lt;BR /&gt;DMA_CHDESC_T Initial_DMA_Descriptor;&lt;/P&gt;&lt;P&gt;ADC_TransferDescriptors[0].source = (uint32_t)&amp;amp;LPC_ADC0-&amp;gt;SEQ_GDAT[0];&lt;BR /&gt;ADC_TransferDescriptors[1].source = (uint32_t)&amp;amp;LPC_ADC0-&amp;gt;SEQ_GDAT[0];&lt;BR /&gt;ADC_TransferDescriptors[2].source = (uint32_t)&amp;amp;LPC_ADC0-&amp;gt;SEQ_GDAT[0];&lt;BR /&gt;ADC_TransferDescriptors[3].source = (uint32_t)&amp;amp;LPC_ADC0-&amp;gt;SEQ_GDAT[0];&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;ADC_TransferDescriptors[0].dest = DMA_ADDR(&amp;amp;CapturedData[(0+1)*DMA_TRANSFER_SIZE-1]);&lt;BR /&gt;ADC_TransferDescriptors[1].dest = DMA_ADDR(&amp;amp;CapturedData[(1+1)*DMA_TRANSFER_SIZE-1]);&lt;BR /&gt;ADC_TransferDescriptors[2].dest = DMA_ADDR(&amp;amp;CapturedData[(2+1)*DMA_TRANSFER_SIZE-1]);&lt;BR /&gt;ADC_TransferDescriptors[3].dest = DMA_ADDR(&amp;amp;CapturedData[(3+1)*DMA_TRANSFER_SIZE-1]);&lt;/P&gt;&lt;P&gt;//The initial DMA desciptor is the same as the 1st transfer descriptor. It&lt;BR /&gt;//Will link into the 2nd of the main descriptors.&lt;/P&gt;&lt;P&gt;ADC_TransferDescriptors[0].next = (uint32_t)&amp;amp;ADC_TransferDescriptors[1];&lt;BR /&gt;ADC_TransferDescriptors[1].next = (uint32_t)&amp;amp;ADC_TransferDescriptors[2];&lt;BR /&gt;ADC_TransferDescriptors[2].next = (uint32_t)&amp;amp;ADC_TransferDescriptors[3];&lt;/P&gt;&lt;P&gt;//Link back to the 1st descriptor&lt;BR /&gt;ADC_TransferDescriptors[3].next = (uint32_t)&amp;amp;ADC_TransferDescriptors[0];&lt;/P&gt;&lt;P&gt;//For a test, stop the transfers here. The sine wave will look fine.&lt;BR /&gt;//ADC_TransferDescriptors[3].next = 0;&lt;/P&gt;&lt;P&gt;ADC_TransferDescriptors[0].xfercfg = (DMA_XFERCFG_CFGVALID |&lt;BR /&gt;DMA_XFERCFG_RELOAD |&lt;BR /&gt;DMA_XFERCFG_SETINTA |&lt;BR /&gt;DMA_XFERCFG_WIDTH_16 |&lt;BR /&gt;DMA_XFERCFG_SRCINC_0 |&lt;BR /&gt;DMA_XFERCFG_DSTINC_1 |&lt;BR /&gt;DMA_XFERCFG_XFERCOUNT(DMA_TRANSFER_SIZE));&lt;/P&gt;&lt;P&gt;ADC_TransferDescriptors[1].xfercfg = ADC_TransferDescriptors[0].xfercfg;&lt;BR /&gt;ADC_TransferDescriptors[2].xfercfg = ADC_TransferDescriptors[0].xfercfg;&lt;/P&gt;&lt;P&gt;ADC_TransferDescriptors[3].xfercfg = (DMA_XFERCFG_CFGVALID |&lt;BR /&gt;DMA_XFERCFG_RELOAD |&lt;BR /&gt;DMA_XFERCFG_SETINTA |&lt;BR /&gt;DMA_XFERCFG_WIDTH_16 |&lt;BR /&gt;DMA_XFERCFG_SRCINC_0 |&lt;BR /&gt;DMA_XFERCFG_DSTINC_1 |&lt;BR /&gt;DMA_XFERCFG_XFERCOUNT(DMA_TRANSFER_SIZE));&lt;/P&gt;&lt;P&gt;Initial_DMA_Descriptor.source = ADC_TransferDescriptors[0].source;&lt;BR /&gt;Initial_DMA_Descriptor.dest = ADC_TransferDescriptors[0].dest;&lt;BR /&gt;Initial_DMA_Descriptor.next = (uint32_t)&amp;amp;ADC_TransferDescriptors[1];&lt;BR /&gt;Initial_DMA_Descriptor.xfercfg = ADC_TransferDescriptors[0].xfercfg;&lt;/P&gt;&lt;P&gt;/* DMA initialization - enable DMA clocking and reset DMA if needed */&lt;BR /&gt;Chip_DMA_Init(LPC_DMA);&lt;/P&gt;&lt;P&gt;/* Enable DMA controller and use driver provided DMA table for current descriptors */&lt;BR /&gt;Chip_DMA_Enable(LPC_DMA);&lt;BR /&gt;Chip_DMA_SetSRAMBase(LPC_DMA, DMA_ADDR(Chip_DMA_Table));&lt;/P&gt;&lt;P&gt;/* Setup channel 0 for the following configuration:&lt;BR /&gt;- High channel priority&lt;BR /&gt;- Interrupt A fires on descriptor completion */&lt;BR /&gt;Chip_DMA_EnableChannel(LPC_DMA, DMA_CH0);&lt;BR /&gt;Chip_DMA_EnableIntChannel(LPC_DMA, DMA_CH0);&lt;BR /&gt;Chip_DMA_SetupChannelConfig(LPC_DMA, DMA_CH0, //(DMA_CFG_PERIPHREQEN |&lt;BR /&gt;(DMA_CFG_HWTRIGEN |&lt;BR /&gt;DMA_CFG_TRIGBURST_BURST |&lt;BR /&gt;DMA_CFG_TRIGTYPE_EDGE |&lt;BR /&gt;DMA_CFG_TRIGPOL_HIGH | //DMA_CFG_TRIGPOL_HIGH&lt;BR /&gt;DMA_CFG_BURSTPOWER_1 |&lt;BR /&gt;DMA_CFG_CHPRIORITY(0)&lt;BR /&gt;)&lt;BR /&gt;);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;//make sure ADC Sequence A interrupts is selected for for a DMA trigger&lt;BR /&gt;Chip_INMUX_SetDMATrigger(DMA_CH0, DMATRIG_ADC0_SEQA_IRQ);&lt;/P&gt;&lt;P&gt;/* Enable DMA interrupt */&lt;BR /&gt;NVIC_EnableIRQ(DMA_IRQn);&lt;/P&gt;&lt;P&gt;// The 1st descriptor is set up through the registers.&lt;/P&gt;&lt;P&gt;/* Setup transfer descriptor and validate it */&lt;BR /&gt;Chip_DMA_SetupTranChannel(LPC_DMA, DMA_CH0, &amp;amp;Initial_DMA_Descriptor);&lt;/P&gt;&lt;P&gt;//Use the transfer configuration for our 4 main descriptors&lt;BR /&gt;Chip_DMA_SetupChannelTransfer(LPC_DMA, DMA_CH0, ADC_TransferDescriptors[0].xfercfg);&lt;BR /&gt;Chip_DMA_SetValidChannel(LPC_DMA, DMA_CH0);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;void SCT_PWM_Generate(void)&lt;BR /&gt;{&lt;BR /&gt;/* Initialize the SCT2 as PWM and set frequency */&lt;BR /&gt;Chip_SCTPWM_Init(LPC_SCT2);&lt;BR /&gt;Chip_SCTPWM_SetRate(LPC_SCT2, SCT_PWM_RATE);&lt;/P&gt;&lt;P&gt;/* Use SCT2_OUT3 pin */&lt;BR /&gt;Chip_SCTPWM_SetOutPin(LPC_SCT2, SCT_PWM_OUT, SCT_PWM_PIN_OUT);&lt;/P&gt;&lt;P&gt;/* Start with 50% duty cycle */&lt;BR /&gt;Chip_SCTPWM_SetDutyCycle(LPC_SCT2, SCT_PWM_OUT, Chip_SCTPWM_PercentageToTicks(LPC_SCT2, 50));&lt;BR /&gt;Chip_SCTPWM_Start(LPC_SCT2);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/***&lt;BR /&gt;* _ ____ ____&lt;BR /&gt;* / \ | _ \ / ___|&lt;BR /&gt;* / _ \ | | | | |&lt;BR /&gt;* / ___ \| |_| | |___&lt;BR /&gt;* /_/__ \_\____/ \____|&lt;BR /&gt;* / ___| ___| |_ _ _ _ __&lt;BR /&gt;* \___ \ / _ \ __| | | | '_ \&lt;BR /&gt;* ___) | __/ |_| |_| | |_) |&lt;BR /&gt;* |____/ \___|\__|\__,_| .__/&lt;BR /&gt;* |_|&lt;BR /&gt;*/&lt;BR /&gt;void ADC_Setup(void)&lt;BR /&gt;{&lt;BR /&gt;/*Set Asynch Clock to the Main clock*/&lt;BR /&gt;// LPC_SYSCON-&amp;gt;ADCCLKSEL = 0;&lt;BR /&gt;// Chip_Clock_SetADCASYNCSource(SYSCTL_ADCASYNCCLKSRC_IRC);&lt;BR /&gt;//Set the divider to 1 and enable. note, the HALT bit (30) and RESET (29) are not in the manual&lt;BR /&gt;// LPC_SYSCON-&amp;gt;ADCCLKDIV = 0;&lt;/P&gt;&lt;P&gt;/* Initialization ADC to 12 bit and set clock divide to 1 to operate synchronously at System clock */&lt;BR /&gt;Chip_ADC_Init(LPC_ADC0, ADC_CR_BITACC(0) | ADC_CR_CLKDIV(0)| ADC_CR_ASYNMODE);&lt;BR /&gt;Chip_ADC_SetClockRate(LPC_ADC0, ADC_MAX_SAMPLE_RATE);&lt;BR /&gt;//select ADC Channel 0 as input&lt;BR /&gt;Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 8, IOCON_FUNC0 | IOCON_MODE_INACT | IOCON_ADMODE_EN);&lt;BR /&gt;Chip_SWM_Init();&lt;BR /&gt;Chip_SWM_EnableFixedPin(SWM_FIXED_ADC0_0); //P0_8&lt;/P&gt;&lt;P&gt;Chip_ADC_SetADC0Input(LPC_ADC0, ADC_INSEL_ADC0);&lt;/P&gt;&lt;P&gt;//Setup ADC0_SEQA_IRQ&lt;BR /&gt;Chip_ADC_SetupSequencer(LPC_ADC0,ADC_SEQA_IDX,&lt;BR /&gt;ADC_SEQ_CTRL_SEQ_ENA |&lt;BR /&gt;ADC_SEQ_CTRL_CHANSEL(ADC_INPUT_CHANNEL) |&lt;BR /&gt;ADC0_SEQ_CTRL_HWTRIG_SCT2_OUT3 |&lt;BR /&gt;// ADC_SEQ_CTRL_HWTRIG_POLPOS |&lt;BR /&gt;// ADC_SEQ_CTRL_HWTRIG_SYNCBYPASS |&lt;BR /&gt;ADC_SEQ_CTRL_MODE_EOS);&lt;BR /&gt;/* Enable Sequence A interrupt */&lt;BR /&gt;Chip_ADC_EnableInt(LPC_ADC0, ADC_INTEN_SEQA_ENABLE);&lt;/P&gt;&lt;P&gt;/* Calibrate ADC */&lt;BR /&gt;Chip_ADC_StartCalibration(LPC_ADC0);&lt;BR /&gt;while (!(Chip_ADC_IsCalibrationDone(LPC_ADC0))) {}&lt;/P&gt;&lt;P&gt;Chip_ADC_ClearFlags(LPC_ADC0, Chip_ADC_GetFlags(LPC_ADC0));&lt;BR /&gt;// Chip_ADC_EnableInt(LPC_ADC0, ADC_INTEN_SEQA_ENABLE);&lt;BR /&gt;// NVIC_EnableIRQ(ADC0_SEQA_IRQn);&lt;BR /&gt;Chip_ADC_EnableSequencer(LPC_ADC0, ADC_SEQA_IDX);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;/* Setup SystemCoreClock and any needed board code */&lt;BR /&gt;SystemCoreClockUpdate();&lt;BR /&gt;Board_Init();&lt;/P&gt;&lt;P&gt;DMA_Setup();&lt;BR /&gt;ADC_Setup();&lt;BR /&gt;SCT_PWM_Generate();&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;while(1)&lt;BR /&gt;{}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 11:41:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-Problem-with-SCT-triggering-ADC-triggering-DMA-at-a/m-p/1211743#M43571</guid>
      <dc:creator>jespermadsen</dc:creator>
      <dc:date>2021-01-14T11:41:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1549: Problem with SCT triggering ADC triggering DMA at a certain frequency</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-Problem-with-SCT-triggering-ADC-triggering-DMA-at-a/m-p/1219029#M43694</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For ADC setup you can refer to the example provided in the LPCOpen, in this example the systick timer is used to trigger the ADC. Also, the SCT timer is initialized but the pins need to be enabled at the beginning of the code.&lt;/P&gt;
&lt;P&gt;It would be helpful if you could measure with an oscilloscope the output of the SCT just to verify that the signal behaves correctly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jan 2021 18:04:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-Problem-with-SCT-triggering-ADC-triggering-DMA-at-a/m-p/1219029#M43694</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-01-21T18:04:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1549: Problem with SCT triggering ADC triggering DMA at a certain frequency</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-Problem-with-SCT-triggering-ADC-triggering-DMA-at-a/m-p/1219439#M43707</link>
      <description>&lt;P&gt;Hello Omar.&lt;/P&gt;&lt;P&gt;I thought this thread got too long down the cue, so I started a new one:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-How-to-use-the-DMA-with-the-ADC/m-p/1216661#M43624" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-How-to-use-the-DMA-with-the-ADC/m-p/1216661#M43624&lt;/A&gt;&lt;/P&gt;&lt;P&gt;with a program that gets the data in the buffer.&lt;/P&gt;&lt;P&gt;Maybe I can delete this one?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jesper&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jan 2021 07:57:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-Problem-with-SCT-triggering-ADC-triggering-DMA-at-a/m-p/1219439#M43707</guid>
      <dc:creator>jespermadsen</dc:creator>
      <dc:date>2021-01-22T07:57:17Z</dc:date>
    </item>
  </channel>
</rss>