<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックAbnormal condition for LPC1519JBD64E</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Abnormal-condition-for-LPC1519JBD64E/m-p/1219129#M43696</link>
    <description>&lt;P&gt;We are using LPC1519 microcontroller. If the user has incorrectly connected the input cable, it is possible that a + 15V (or minus 15V) battery may be connected to one of the PIO1 inputs (pin 51) through a 5.7K resistor. In this state, no other voltages will be applied to this microcontroller. Thus, the maximum possible current is less than 3 mA. Is it safe for the microcontroller or does it require additional protection?&lt;/P&gt;</description>
    <pubDate>Thu, 21 Jan 2021 23:03:10 GMT</pubDate>
    <dc:creator>lev_nemets</dc:creator>
    <dc:date>2021-01-21T23:03:10Z</dc:date>
    <item>
      <title>Abnormal condition for LPC1519JBD64E</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Abnormal-condition-for-LPC1519JBD64E/m-p/1219129#M43696</link>
      <description>&lt;P&gt;We are using LPC1519 microcontroller. If the user has incorrectly connected the input cable, it is possible that a + 15V (or minus 15V) battery may be connected to one of the PIO1 inputs (pin 51) through a 5.7K resistor. In this state, no other voltages will be applied to this microcontroller. Thus, the maximum possible current is less than 3 mA. Is it safe for the microcontroller or does it require additional protection?&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jan 2021 23:03:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Abnormal-condition-for-LPC1519JBD64E/m-p/1219129#M43696</guid>
      <dc:creator>lev_nemets</dc:creator>
      <dc:date>2021-01-21T23:03:10Z</dc:date>
    </item>
    <item>
      <title>Re: Abnormal condition for LPC1519JBD64E</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Abnormal-condition-for-LPC1519JBD64E/m-p/1219320#M43699</link>
      <description>&lt;P&gt;Hi, Lev,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Pls refer to the following section limiting values in data sheet of LPC15xx. The I/O maximum voltage is 5.5V under the condition&amp;nbsp; VDD&amp;gt;2.4V. The I/O maximum voltage is 3.3V under the condition&amp;nbsp; the VDD=0V.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BTW, for almost each pins, there are internal protection diode specifically designed for the protection of its internal devices from the damaging effects of excessive&lt;BR /&gt;static charge. The current must be less than 3mA as far as I know, if the I/O pin is exposed to 15V voltage with serial resistor in a short time, I think it is okay. But I suppose we never have a test for the scenario.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_1-1611291342435.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135526iA612DE25C534A210/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_1-1611291342435.png" alt="xiangjun_rong_1-1611291342435.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_1-1611291342435.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;[1] The following applies to the limiting values:&lt;BR /&gt;a) This product includes circuitry specifically designed for the protection of its internal devices from the damaging effects of excessive&lt;BR /&gt;static charge. Nonetheless, it is suggested that conventional precautions be taken to avoid applying greater than the rated&lt;BR /&gt;maximum.&lt;BR /&gt;b) Parameters are valid over operating temperature range unless otherwise specified. All voltages are with respect to VSS unless&lt;BR /&gt;otherwise noted.&lt;/P&gt;
&lt;DIV id="tinyMceEditorxiangjun_rong_2" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV id="tinyMceEditorxiangjun_rong_3" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jan 2021 05:10:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Abnormal-condition-for-LPC1519JBD64E/m-p/1219320#M43699</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-01-22T05:10:53Z</dc:date>
    </item>
  </channel>
</rss>