<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC55S28 USB MSD host enumeration failed</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-USB-MSD-host-enumeration-failed/m-p/1218868#M43690</link>
    <description>&lt;P&gt;Hallo,&lt;/P&gt;&lt;P&gt;I'm developing a custum project using LPC55s28 microcontroller and MCUXpresso IDE vs&amp;nbsp;IDE v11.2.1 ,Build 4149, 2020-10-07.&lt;/P&gt;&lt;P&gt;I need insert the USB MSD driver and I took it from the lpcxpresso55s28_host_msd_fatfs_freertos example because I'm using the freertos OS.&lt;/P&gt;&lt;P&gt;I'm using the USB type A insted of the USB type C connector.&lt;BR /&gt;I'm using the USB0 peripheral and I configured the USB0_VBUS on the PIO1_11 pin. The USB peripheral clock source is the FRO (96MHz) and I set the USB clock divider to 2. The clock status register gives me the information that it's working correctly.&lt;/P&gt;&lt;P&gt;I configured the PIO1_11 as USB0_VBUS and connected it to 3,3V and I'm not using the USB0_IDVALUE pin.&lt;/P&gt;&lt;P&gt;When I plug USB stick in, the software recognizes the event, enters in the&amp;nbsp;USB_HostEnumerationTransferCallback function and returns from it with the enumeration failed event.&amp;nbsp; Than software enters in the KUSB_HostEventEnumerationFail case of the USB_HostEvent function.&lt;BR /&gt;Moreover I had to disable the USB_HostOhciDelay in the USB_HostOhciPortChange function, because when I plug the USB stick in, it's caused a software breakpoint event in the software.&lt;/P&gt;&lt;P&gt;I changed many USB stick, and I&amp;nbsp;checked the software many times but I haven't found the problem source.&lt;/P&gt;&lt;P&gt;Could someone help me to solve the problem or give me a tip?&lt;/P&gt;&lt;P&gt;Many thanks in advance.&lt;/P&gt;&lt;P&gt;Kinds Regards,&lt;/P&gt;&lt;P&gt;Chobin&lt;/P&gt;</description>
    <pubDate>Thu, 21 Jan 2021 14:48:03 GMT</pubDate>
    <dc:creator>chobin</dc:creator>
    <dc:date>2021-01-21T14:48:03Z</dc:date>
    <item>
      <title>LPC55S28 USB MSD host enumeration failed</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-USB-MSD-host-enumeration-failed/m-p/1218868#M43690</link>
      <description>&lt;P&gt;Hallo,&lt;/P&gt;&lt;P&gt;I'm developing a custum project using LPC55s28 microcontroller and MCUXpresso IDE vs&amp;nbsp;IDE v11.2.1 ,Build 4149, 2020-10-07.&lt;/P&gt;&lt;P&gt;I need insert the USB MSD driver and I took it from the lpcxpresso55s28_host_msd_fatfs_freertos example because I'm using the freertos OS.&lt;/P&gt;&lt;P&gt;I'm using the USB type A insted of the USB type C connector.&lt;BR /&gt;I'm using the USB0 peripheral and I configured the USB0_VBUS on the PIO1_11 pin. The USB peripheral clock source is the FRO (96MHz) and I set the USB clock divider to 2. The clock status register gives me the information that it's working correctly.&lt;/P&gt;&lt;P&gt;I configured the PIO1_11 as USB0_VBUS and connected it to 3,3V and I'm not using the USB0_IDVALUE pin.&lt;/P&gt;&lt;P&gt;When I plug USB stick in, the software recognizes the event, enters in the&amp;nbsp;USB_HostEnumerationTransferCallback function and returns from it with the enumeration failed event.&amp;nbsp; Than software enters in the KUSB_HostEventEnumerationFail case of the USB_HostEvent function.&lt;BR /&gt;Moreover I had to disable the USB_HostOhciDelay in the USB_HostOhciPortChange function, because when I plug the USB stick in, it's caused a software breakpoint event in the software.&lt;/P&gt;&lt;P&gt;I changed many USB stick, and I&amp;nbsp;checked the software many times but I haven't found the problem source.&lt;/P&gt;&lt;P&gt;Could someone help me to solve the problem or give me a tip?&lt;/P&gt;&lt;P&gt;Many thanks in advance.&lt;/P&gt;&lt;P&gt;Kinds Regards,&lt;/P&gt;&lt;P&gt;Chobin&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jan 2021 14:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-USB-MSD-host-enumeration-failed/m-p/1218868#M43690</guid>
      <dc:creator>chobin</dc:creator>
      <dc:date>2021-01-21T14:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28 USB MSD host enumeration failed</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-USB-MSD-host-enumeration-failed/m-p/1220803#M43735</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/2908"&gt;@chobin&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing well!&lt;/P&gt;
&lt;P&gt;Regarding the hardware setup.&lt;/P&gt;
&lt;P&gt;Are you able to post an USB schematic of your design with component values?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Is the USB host able to enumerate any other kind of device such as keyboard or mouse?&lt;/P&gt;
&lt;P&gt;If it helps,&amp;nbsp; in the MCUxpresso SDK release notes, you will find USB drives that have been tested with the USB stack.&lt;/P&gt;
&lt;P&gt;Yours&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 20:01:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-USB-MSD-host-enumeration-failed/m-p/1220803#M43735</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2021-01-25T20:01:41Z</dc:date>
    </item>
  </channel>
</rss>