<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC54018 linker file question regarding SRAM addresses in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-linker-file-question-regarding-SRAM-addresses/m-p/1218279#M43668</link>
    <description>&lt;P&gt;I'm writing software for the&amp;nbsp;LPC54018J4MET180 and using Keil MDK for development.&amp;nbsp; The NXP DFP includes a default linker (scatter) file and there is something I don't understand.&lt;/P&gt;&lt;P&gt;When not running an image from flash, the SRAM (m_data) range is defined as 0x20000000 -&amp;nbsp;0x20028000.&amp;nbsp; This is a continuous bank of SRAM and this makes sense.&lt;/P&gt;&lt;P&gt;When running an image from flash (XIP), the SRAM range is 0x00000004 - 0x00030000.&amp;nbsp; This is a different bank of SRAM, but can anyone tell me why it doesn't start at address zero?&amp;nbsp; Are the first four bytes being used for something else?&amp;nbsp; I've looked but cannot find any reason for this.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-left" image-alt="sram.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135356i77DC18FC62246341/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sram.png" alt="sram.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;sram.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any help!!&lt;/P&gt;</description>
    <pubDate>Wed, 20 Jan 2021 21:55:56 GMT</pubDate>
    <dc:creator>rawsewage</dc:creator>
    <dc:date>2021-01-20T21:55:56Z</dc:date>
    <item>
      <title>LPC54018 linker file question regarding SRAM addresses</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-linker-file-question-regarding-SRAM-addresses/m-p/1218279#M43668</link>
      <description>&lt;P&gt;I'm writing software for the&amp;nbsp;LPC54018J4MET180 and using Keil MDK for development.&amp;nbsp; The NXP DFP includes a default linker (scatter) file and there is something I don't understand.&lt;/P&gt;&lt;P&gt;When not running an image from flash, the SRAM (m_data) range is defined as 0x20000000 -&amp;nbsp;0x20028000.&amp;nbsp; This is a continuous bank of SRAM and this makes sense.&lt;/P&gt;&lt;P&gt;When running an image from flash (XIP), the SRAM range is 0x00000004 - 0x00030000.&amp;nbsp; This is a different bank of SRAM, but can anyone tell me why it doesn't start at address zero?&amp;nbsp; Are the first four bytes being used for something else?&amp;nbsp; I've looked but cannot find any reason for this.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-left" image-alt="sram.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135356i77DC18FC62246341/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sram.png" alt="sram.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;sram.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any help!!&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 21:55:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-linker-file-question-regarding-SRAM-addresses/m-p/1218279#M43668</guid>
      <dc:creator>rawsewage</dc:creator>
      <dc:date>2021-01-20T21:55:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 linker file question regarding SRAM addresses</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-linker-file-question-regarding-SRAM-addresses/m-p/1218580#M43676</link>
      <description>&lt;P&gt;Hello Greg,&lt;/P&gt;
&lt;P&gt;I think you change it to 0x00000000 also will be OK, you can test it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jan 2021 07:16:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-linker-file-question-regarding-SRAM-addresses/m-p/1218580#M43676</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-01-21T07:16:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 linker file question regarding SRAM addresses</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-linker-file-question-regarding-SRAM-addresses/m-p/1222822#M43767</link>
      <description>&lt;P&gt;Thanks, everything works fine as expected.&amp;nbsp; I just wanted to make sure I wasn't missing anything.&amp;nbsp; Perhaps the scatter file should be updated in the NXP DFP.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jan 2021 18:41:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-linker-file-question-regarding-SRAM-addresses/m-p/1222822#M43767</guid>
      <dc:creator>rawsewage</dc:creator>
      <dc:date>2021-01-28T18:41:26Z</dc:date>
    </item>
  </channel>
</rss>