<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC55S69 Execute ISP Command</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Execute-ISP-Command/m-p/1211906#M43574</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;When I send the "execute" command to the ISP ROM bootloader, the LPC55S69 responds with "Command is Not Supported (0x2716). The user manual claims that this is a supported command, and "get-property available-commands" shows that execute is a valid command. What am I doing wrong? I am trying to execute a program that I have loaded into RAM via an SB2.1 upload.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;</description>
    <pubDate>Thu, 14 Jan 2021 18:50:36 GMT</pubDate>
    <dc:creator>awseiger</dc:creator>
    <dc:date>2021-01-14T18:50:36Z</dc:date>
    <item>
      <title>LPC55S69 Execute ISP Command</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Execute-ISP-Command/m-p/1211906#M43574</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;When I send the "execute" command to the ISP ROM bootloader, the LPC55S69 responds with "Command is Not Supported (0x2716). The user manual claims that this is a supported command, and "get-property available-commands" shows that execute is a valid command. What am I doing wrong? I am trying to execute a program that I have loaded into RAM via an SB2.1 upload.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 18:50:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Execute-ISP-Command/m-p/1211906#M43574</guid>
      <dc:creator>awseiger</dc:creator>
      <dc:date>2021-01-14T18:50:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 Execute ISP Command</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Execute-ISP-Command/m-p/1212024#M43576</link>
      <description>&lt;P&gt;Hello Alex,&lt;/P&gt;
&lt;P&gt;Do you use blhost ?&lt;/P&gt;
&lt;P&gt;Could you please show all your steps and all the commands?&lt;/P&gt;
&lt;P&gt;If you want to use secure boot, recommend you refer to this application note:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12283.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12283.pdf&lt;/A&gt;&amp;nbsp; &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jan 2021 02:03:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Execute-ISP-Command/m-p/1212024#M43576</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-01-15T02:03:54Z</dc:date>
    </item>
  </channel>
</rss>