<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLIN Master Mode Break generation</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LIN-Master-Mode-Break-generation/m-p/1211542#M43566</link>
    <description>&lt;P&gt;The Manual said:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wangyanjun_0-1610606300005.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/134741i7DA0B19B23E03B2E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="wangyanjun_0-1610606300005.png" alt="wangyanjun_0-1610606300005.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;My questions are:&lt;/P&gt;&lt;P&gt;1. In LIN master mode, the break signal is not continuous, and after 13 bit time, tx pin will restore to high automatically, is this right?&lt;/P&gt;&lt;P&gt;2. In LIN master mode, if DELTARXBRK interrupt is enabled, there will be 2 times interrupt, first is after 11 bit time from the TXBRKEN is set, second is after 13 bit time when tx pin restore to high. Is this right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Thu, 14 Jan 2021 06:48:47 GMT</pubDate>
    <dc:creator>wangyanjun</dc:creator>
    <dc:date>2021-01-14T06:48:47Z</dc:date>
    <item>
      <title>LIN Master Mode Break generation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LIN-Master-Mode-Break-generation/m-p/1211542#M43566</link>
      <description>&lt;P&gt;The Manual said:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wangyanjun_0-1610606300005.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/134741i7DA0B19B23E03B2E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="wangyanjun_0-1610606300005.png" alt="wangyanjun_0-1610606300005.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;My questions are:&lt;/P&gt;&lt;P&gt;1. In LIN master mode, the break signal is not continuous, and after 13 bit time, tx pin will restore to high automatically, is this right?&lt;/P&gt;&lt;P&gt;2. In LIN master mode, if DELTARXBRK interrupt is enabled, there will be 2 times interrupt, first is after 11 bit time from the TXBRKEN is set, second is after 13 bit time when tx pin restore to high. Is this right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 06:48:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LIN-Master-Mode-Break-generation/m-p/1211542#M43566</guid>
      <dc:creator>wangyanjun</dc:creator>
      <dc:date>2021-01-14T06:48:47Z</dc:date>
    </item>
    <item>
      <title>Re: LIN Master Mode Break generation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LIN-Master-Mode-Break-generation/m-p/1213540#M43607</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1. Yes, that is correct.&lt;/P&gt;
&lt;P&gt;2. If you enable DELTARXBRKEN then you can check you can check UART_STAT[DELTARXBRK] and UART_STAT[RXBRK] when LIN break happens. This will be after RX input remains low for 11 bit.&lt;/P&gt;
&lt;P&gt;In addition I recommend you to check the following community document from a colleague that provides an example of using LIN master in LPC546x MCUs.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC54608-LIN-master-basic-usage-sharing/ta-p/1118103" target="_blank"&gt;LPC54608 LIN master basic usage sharing - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jan 2021 17:49:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LIN-Master-Mode-Break-generation/m-p/1213540#M43607</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-01-18T17:49:52Z</dc:date>
    </item>
  </channel>
</rss>