<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC55S69 SPI Flash Recovery Boot Configuration</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-SPI-Flash-Recovery-Boot-Configuration/m-p/1210630#M43553</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to configure the SPI Flash Recovery Boot on the LPC55S69. Documentation points to bits 3:0 in the CMPA (Address 0x9E404), but does not specify what these bits need to be. I tried 0x00 through 0x0F and the bootloader did not load the SB2.1 file I wrote to address 0x0 on my connected SPI Flash.&lt;/P&gt;&lt;P&gt;Could you provide some documentation as to how one should configure the LPC55S69 to load an SB2.1 image from SPI Flash?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Alex&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 12 Jan 2021 22:04:03 GMT</pubDate>
    <dc:creator>awseiger</dc:creator>
    <dc:date>2021-01-12T22:04:03Z</dc:date>
    <item>
      <title>LPC55S69 SPI Flash Recovery Boot Configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-SPI-Flash-Recovery-Boot-Configuration/m-p/1210630#M43553</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to configure the SPI Flash Recovery Boot on the LPC55S69. Documentation points to bits 3:0 in the CMPA (Address 0x9E404), but does not specify what these bits need to be. I tried 0x00 through 0x0F and the bootloader did not load the SB2.1 file I wrote to address 0x0 on my connected SPI Flash.&lt;/P&gt;&lt;P&gt;Could you provide some documentation as to how one should configure the LPC55S69 to load an SB2.1 image from SPI Flash?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Alex&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jan 2021 22:04:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-SPI-Flash-Recovery-Boot-Configuration/m-p/1210630#M43553</guid>
      <dc:creator>awseiger</dc:creator>
      <dc:date>2021-01-12T22:04:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 SPI Flash Recovery Boot Configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-SPI-Flash-Recovery-Boot-Configuration/m-p/1216450#M43615</link>
      <description>&lt;P&gt;Hello Alex,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="caseEventBody"&gt;&lt;SPAN class="caseEventRow"&gt;&lt;SPAN class="feeditemtext cxfeeditemtext"&gt;"if SPI_RECOVERY_BOOT_EN not '0000' then enable SPI recovery.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;And do you use LPC55s69-EVK board? If yes, there is no external flash in board.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 02:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-SPI-Flash-Recovery-Boot-Configuration/m-p/1216450#M43615</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-01-19T02:41:59Z</dc:date>
    </item>
  </channel>
</rss>