<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC54616 SCTimer input</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616-SCTimer-input/m-p/1210035#M43533</link>
    <description>&lt;P&gt;As described in the manual, Tx_OUT0 can be used as SCTimer input.&lt;/P&gt;&lt;P&gt;But what is the Tx_OUT0? Is CTimer's match output or others?&lt;/P&gt;</description>
    <pubDate>Tue, 12 Jan 2021 03:15:32 GMT</pubDate>
    <dc:creator>wangyanjun</dc:creator>
    <dc:date>2021-01-12T03:15:32Z</dc:date>
    <item>
      <title>LPC54616 SCTimer input</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616-SCTimer-input/m-p/1210035#M43533</link>
      <description>&lt;P&gt;As described in the manual, Tx_OUT0 can be used as SCTimer input.&lt;/P&gt;&lt;P&gt;But what is the Tx_OUT0? Is CTimer's match output or others?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jan 2021 03:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616-SCTimer-input/m-p/1210035#M43533</guid>
      <dc:creator>wangyanjun</dc:creator>
      <dc:date>2021-01-12T03:15:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54616 SCTimer input</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616-SCTimer-input/m-p/1210159#M43537</link>
      <description>&lt;P&gt;Hi, YanJun,&lt;/P&gt;
&lt;P&gt;As the following Fig shows, the Tx_OUT0 can be an input signal for the SCT module, the signal can function as capture signal, which can generate event with programmable rising/falling edges, if you enable an interrupt, the event can trigger an interrupt. With the capture function, user can test the width of the signal..&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1610435435898.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/134503i5DBDEFADB43E6DD8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1610435435898.png" alt="xiangjun_rong_0-1610435435898.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1610435435898.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 06:45:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616-SCTimer-input/m-p/1210159#M43537</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-01-14T06:45:55Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54616 SCTimer input</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616-SCTimer-input/m-p/1211519#M43565</link>
      <description>&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;I found the answer from MCUxpresso Config Tools. The Tx_OUT0 is the CTimer's match channel 0 output.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 06:27:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616-SCTimer-input/m-p/1211519#M43565</guid>
      <dc:creator>wangyanjun</dc:creator>
      <dc:date>2021-01-14T06:27:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54616 SCTimer input</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616-SCTimer-input/m-p/1211546#M43567</link>
      <description>&lt;P&gt;Hi, YanJun,&lt;/P&gt;
&lt;P&gt;Thank you for the feedback. If the CTimer is used to counts external clock, and you want to test the external signal clock frequency, you can use the CTimer as a divider, the CTimer outputting clock signal can function&amp;nbsp;as a capture signal for the SCT, with the capture function, the SCT can test the external signal frequency.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 06:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616-SCTimer-input/m-p/1211546#M43567</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-01-14T06:51:59Z</dc:date>
    </item>
  </channel>
</rss>