<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックExternal Clock Frequency range LPC55Sxx</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/External-Clock-Frequency-range-LPC55Sxx/m-p/1209916#M43532</link>
    <description>&lt;P&gt;I am unclear as to the range of frequencies that can be applied as an external clock.&lt;BR /&gt;I wish to use an external TCVCXO at 10.0000MHz as the system clock.&lt;/P&gt;&lt;P&gt;UM11126 Section 1.2 under clock generation says&lt;BR /&gt;&lt;EM&gt;&lt;SPAN&gt;"&amp;nbsp;Crystal oscillator with an operating frequency of &lt;STRONG&gt;12 MHz&lt;/STRONG&gt; to 32 MHz. Option for&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;external clock input (bypass mode) for clock frequencies of up to 24 MHz"&lt;/SPAN&gt;&lt;/EM&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;LPC55S6x Data sheet (7.22.1) says&lt;BR /&gt;&lt;EM&gt;&lt;SPAN&gt;Crystal oscillator with an operating frequency of &lt;STRONG&gt;1 MHz&lt;/STRONG&gt; to 32 MHz. Option for external&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;EM&gt;&lt;SPAN&gt;clock input (bypass mode) for clock frequencies of up to 24 MHz&lt;/SPAN&gt;&lt;/EM&gt;&lt;EM&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;EM&gt;&lt;SPAN&gt;Also&lt;BR /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;EM&gt;In bypass mode, an external clock (maximum frequency of up to 24 MHz) can also be&lt;BR /&gt;connected to XTAL32M_P if XTAL32M_N is left open. External [0 – VH] square signal can&lt;BR /&gt;be applied on the XTAL32M_P pin from 0 V to 850 mV.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Playing with the clock configuration tool, I cannot set a crystal value of &amp;lt; 12MHz in "Normal crystal oscillation mode.", however by selecting "External clock input (bypass mode)." mode - I can set it to 10MHz.&lt;BR /&gt;I am presuming that external clock source can be 1MHz to 24MHz, and the Crystal can be 12MHz to 32MHz&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this correct??&lt;/P&gt;</description>
    <pubDate>Tue, 12 Jan 2021 00:06:35 GMT</pubDate>
    <dc:creator>Watarat</dc:creator>
    <dc:date>2021-01-12T00:06:35Z</dc:date>
    <item>
      <title>External Clock Frequency range LPC55Sxx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/External-Clock-Frequency-range-LPC55Sxx/m-p/1209916#M43532</link>
      <description>&lt;P&gt;I am unclear as to the range of frequencies that can be applied as an external clock.&lt;BR /&gt;I wish to use an external TCVCXO at 10.0000MHz as the system clock.&lt;/P&gt;&lt;P&gt;UM11126 Section 1.2 under clock generation says&lt;BR /&gt;&lt;EM&gt;&lt;SPAN&gt;"&amp;nbsp;Crystal oscillator with an operating frequency of &lt;STRONG&gt;12 MHz&lt;/STRONG&gt; to 32 MHz. Option for&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;external clock input (bypass mode) for clock frequencies of up to 24 MHz"&lt;/SPAN&gt;&lt;/EM&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;LPC55S6x Data sheet (7.22.1) says&lt;BR /&gt;&lt;EM&gt;&lt;SPAN&gt;Crystal oscillator with an operating frequency of &lt;STRONG&gt;1 MHz&lt;/STRONG&gt; to 32 MHz. Option for external&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;EM&gt;&lt;SPAN&gt;clock input (bypass mode) for clock frequencies of up to 24 MHz&lt;/SPAN&gt;&lt;/EM&gt;&lt;EM&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;EM&gt;&lt;SPAN&gt;Also&lt;BR /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;EM&gt;In bypass mode, an external clock (maximum frequency of up to 24 MHz) can also be&lt;BR /&gt;connected to XTAL32M_P if XTAL32M_N is left open. External [0 – VH] square signal can&lt;BR /&gt;be applied on the XTAL32M_P pin from 0 V to 850 mV.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Playing with the clock configuration tool, I cannot set a crystal value of &amp;lt; 12MHz in "Normal crystal oscillation mode.", however by selecting "External clock input (bypass mode)." mode - I can set it to 10MHz.&lt;BR /&gt;I am presuming that external clock source can be 1MHz to 24MHz, and the Crystal can be 12MHz to 32MHz&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this correct??&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jan 2021 00:06:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/External-Clock-Frequency-range-LPC55Sxx/m-p/1209916#M43532</guid>
      <dc:creator>Watarat</dc:creator>
      <dc:date>2021-01-12T00:06:35Z</dc:date>
    </item>
    <item>
      <title>Re: External Clock Frequency range LPC55Sxx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/External-Clock-Frequency-range-LPC55Sxx/m-p/1210106#M43536</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;You are right.&amp;nbsp;&lt;SPAN&gt;external clock source can be 1MHz to 24MHz, and the Crystal can be 12MHz to 32MHz.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jan 2021 06:40:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/External-Clock-Frequency-range-LPC55Sxx/m-p/1210106#M43536</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-01-12T06:40:52Z</dc:date>
    </item>
  </channel>
</rss>