<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC845_SSD1306_IIC_I2C_APPLICATION_EXAMPLE in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-SSD1306-IIC-I2C-APPLICATION-EXAMPLE/m-p/1209656#M43523</link>
    <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I'm working on a project using an OLED screen (SSD1306 - 128*64 - with I2C). i based my work on the example " LPC845_BOB_OLED" that uses the same screen but with SPI. I was searching for a solution with I2C but i couldn't find it. Here is my solution:&lt;/P&gt;&lt;P&gt;&lt;U&gt;Modified library: (&lt;/U&gt;it goes to the DRIVER folder)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;*fsl_ssd1306_i2c.c&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;*fsl_ssd1306_i2c.h&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;*fsl_Font5x7.h&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;NOTE1:&amp;nbsp; this files are working with the I2C1, if you want to use another change I2C1, wherever it appears, with the one that you are using.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;U&gt;Source file:&lt;/U&gt; (it goes to the SOURCE folder)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;*LPC845_SSD1306_OLED.c&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;NOTE2: the power supply that i was using was 3.3V and with 10K pullup resistors in SDA and SCL.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 11 Jan 2021 12:59:08 GMT</pubDate>
    <dc:creator>LeonardoP4</dc:creator>
    <dc:date>2021-01-11T12:59:08Z</dc:date>
    <item>
      <title>LPC845_SSD1306_IIC_I2C_APPLICATION_EXAMPLE</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-SSD1306-IIC-I2C-APPLICATION-EXAMPLE/m-p/1209656#M43523</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I'm working on a project using an OLED screen (SSD1306 - 128*64 - with I2C). i based my work on the example " LPC845_BOB_OLED" that uses the same screen but with SPI. I was searching for a solution with I2C but i couldn't find it. Here is my solution:&lt;/P&gt;&lt;P&gt;&lt;U&gt;Modified library: (&lt;/U&gt;it goes to the DRIVER folder)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;*fsl_ssd1306_i2c.c&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;*fsl_ssd1306_i2c.h&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;*fsl_Font5x7.h&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;NOTE1:&amp;nbsp; this files are working with the I2C1, if you want to use another change I2C1, wherever it appears, with the one that you are using.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;U&gt;Source file:&lt;/U&gt; (it goes to the SOURCE folder)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;*LPC845_SSD1306_OLED.c&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;NOTE2: the power supply that i was using was 3.3V and with 10K pullup resistors in SDA and SCL.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 12:59:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-SSD1306-IIC-I2C-APPLICATION-EXAMPLE/m-p/1209656#M43523</guid>
      <dc:creator>LeonardoP4</dc:creator>
      <dc:date>2021-01-11T12:59:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845_SSD1306_IIC_I2C_APPLICATION_EXAMPLE</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-SSD1306-IIC-I2C-APPLICATION-EXAMPLE/m-p/1209661#M43525</link>
      <description>&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/OLED-Display-Application-Example-using-LPC845-Breakout-Board-and/ta-p/1129277" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/OLED-Display-Application-Example-using-LPC845-Breakout-Board-and/ta-p/1129277&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Here is the SPI application.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 13:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-SSD1306-IIC-I2C-APPLICATION-EXAMPLE/m-p/1209661#M43525</guid>
      <dc:creator>LeonardoP4</dc:creator>
      <dc:date>2021-01-11T13:05:23Z</dc:date>
    </item>
  </channel>
</rss>