<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S69 I2S Record (Rx) examples</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-I2S-Record-Rx-examples/m-p/1209631#M43521</link>
    <description>&lt;P&gt;Thanks Jun Zhang,&lt;/P&gt;&lt;P&gt;I was looking at the wrong SDK, which is why I could only see Tx.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Mon, 11 Jan 2021 11:38:48 GMT</pubDate>
    <dc:creator>sanders7284</dc:creator>
    <dc:date>2021-01-11T11:38:48Z</dc:date>
    <item>
      <title>LPC55S69 I2S Record (Rx) examples</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-I2S-Record-Rx-examples/m-p/1208845#M43493</link>
      <description>&lt;P&gt;Trying to interface to a CMX655D codec via I2S.&lt;/P&gt;&lt;P&gt;I have all the right signals int the right places and have checked all the IRQ are enabled in the NVIC and Flexcomm. Despite this I have no IRQ being generated.&lt;/P&gt;&lt;P&gt;Just wondering if there are any examples of I2S Record (Rx) all the SDK examples are play (Tx). &amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 09:25:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-I2S-Record-Rx-examples/m-p/1208845#M43493</guid>
      <dc:creator>sanders7284</dc:creator>
      <dc:date>2021-01-08T09:25:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 I2S Record (Rx) examples</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-I2S-Record-Rx-examples/m-p/1209384#M43512</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer MCUXpresso I2S SDK demo code&lt;/P&gt;
&lt;P&gt;SDK_2.8.2_LPCXpresso55S69\boards\lpcxpresso55s69\driver_examples\i2s&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 05:02:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-I2S-Record-Rx-examples/m-p/1209384#M43512</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-01-11T05:02:30Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 I2S Record (Rx) examples</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-I2S-Record-Rx-examples/m-p/1209631#M43521</link>
      <description>&lt;P&gt;Thanks Jun Zhang,&lt;/P&gt;&lt;P&gt;I was looking at the wrong SDK, which is why I could only see Tx.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 11:38:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-I2S-Record-Rx-examples/m-p/1209631#M43521</guid>
      <dc:creator>sanders7284</dc:creator>
      <dc:date>2021-01-11T11:38:48Z</dc:date>
    </item>
  </channel>
</rss>