<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55 SB2.1 recovery Image loading from SPI - Is a physical reset required? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-SB2-1-recovery-Image-loading-from-SPI-Is-a-physical-reset/m-p/1209093#M43504</link>
    <description>&lt;P&gt;I am reading documentation on the LPC55 SB2.1 recovery image load from SPI Flash - My company wishes to use this system for field updates.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Once the SPI Flash recovery from an SB2.1 image is complete, does the MCU automatically run the new image, or is a physical reset required?&lt;/P&gt;</description>
    <pubDate>Fri, 08 Jan 2021 18:55:31 GMT</pubDate>
    <dc:creator>awseiger</dc:creator>
    <dc:date>2021-01-08T18:55:31Z</dc:date>
    <item>
      <title>LPC55 SB2.1 recovery Image loading from SPI - Is a physical reset required?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-SB2-1-recovery-Image-loading-from-SPI-Is-a-physical-reset/m-p/1209093#M43504</link>
      <description>&lt;P&gt;I am reading documentation on the LPC55 SB2.1 recovery image load from SPI Flash - My company wishes to use this system for field updates.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Once the SPI Flash recovery from an SB2.1 image is complete, does the MCU automatically run the new image, or is a physical reset required?&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 18:55:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-SB2-1-recovery-Image-loading-from-SPI-Is-a-physical-reset/m-p/1209093#M43504</guid>
      <dc:creator>awseiger</dc:creator>
      <dc:date>2021-01-08T18:55:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55 SB2.1 recovery Image loading from SPI - Is a physical reset required?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-SB2-1-recovery-Image-loading-from-SPI-Is-a-physical-reset/m-p/1209400#M43513</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Reset is not needed.&lt;/P&gt;
&lt;P&gt;But you need make sure SB2.1 file is stored&amp;nbsp; in SPI Flash and secure boot is enabled if using SPI flash recovery feature.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 05:35:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-SB2-1-recovery-Image-loading-from-SPI-Is-a-physical-reset/m-p/1209400#M43513</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-01-11T05:35:07Z</dc:date>
    </item>
  </channel>
</rss>