<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: SB2.1 Image Load from Code</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SB2-1-Image-Load-from-Code/m-p/1208733#M43488</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;SB2.1 file is sign+encrypted image generated by elftosb from plain image. This is a boot images supported by LPC55Sxx.We must use it with secure boot via ISP. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;We can’t decode it and program with source code. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you want to program flash inside source code, please use plain image directly.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For more about sb2.1 file and secure boot, see AN12283.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 08 Jan 2021 06:10:13 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2021-01-08T06:10:13Z</dc:date>
    <item>
      <title>SB2.1 Image Load from Code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SB2-1-Image-Load-from-Code/m-p/1208543#M43483</link>
      <description>&lt;P&gt;I am trying to implement a reliable bootloader system that utilizes the NXP SB2.1 image format. To do this, I need to be able to do the following:&lt;/P&gt;&lt;P&gt;1. Generate an SB2.1 image from the currently-executing program to be stored in off-chip SPI flash for ROM bootloader recovery&lt;/P&gt;&lt;P&gt;2. Decode an SB2.1 image stored in another section of SPI Flash and copy it to the boot space.&lt;/P&gt;&lt;P&gt;I cannot find a way to load an SB2.1 file into the ROM bootloader through anything but the blhost interface, and in my desired implementation I need to do this in software internal to the LPC55.&lt;/P&gt;&lt;P&gt;Is the code for generating/decoding an SB2.1 file available? If so I can write our bootloader code to encode/decode these files.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 22:40:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SB2-1-Image-Load-from-Code/m-p/1208543#M43483</guid>
      <dc:creator>awseiger</dc:creator>
      <dc:date>2021-01-07T22:40:38Z</dc:date>
    </item>
    <item>
      <title>Re: SB2.1 Image Load from Code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SB2-1-Image-Load-from-Code/m-p/1208733#M43488</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;SB2.1 file is sign+encrypted image generated by elftosb from plain image. This is a boot images supported by LPC55Sxx.We must use it with secure boot via ISP. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;We can’t decode it and program with source code. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you want to program flash inside source code, please use plain image directly.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For more about sb2.1 file and secure boot, see AN12283.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 06:10:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SB2-1-Image-Load-from-Code/m-p/1208733#M43488</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-01-08T06:10:13Z</dc:date>
    </item>
    <item>
      <title>Re: SB2.1 Image Load from Code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SB2-1-Image-Load-from-Code/m-p/1208991#M43499</link>
      <description>&lt;P&gt;Is there a better explanation of the SB2.1 format? AN12283 does not have a detailed description of the format and how it works.&lt;/P&gt;&lt;P&gt;Also, is there a way to access the SB2.1 firmware load commands via the same interface the ROM-Based flash driver uses?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 14:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SB2-1-Image-Load-from-Code/m-p/1208991#M43499</guid>
      <dc:creator>awseiger</dc:creator>
      <dc:date>2021-01-08T14:18:13Z</dc:date>
    </item>
  </channel>
</rss>