<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC2468FBD208 revB failed ICT</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1208152#M43476</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can someone help me to solve the problem I encountered during ICT ? Using rev.B of this device zener diode voltage is pulled low but when using rev.D, ICT passed. I checked the errata sheet and cannot find any information related to this.&lt;/P&gt;&lt;P&gt;Additional question, does rev.B and rev.D have different device ID ?&lt;/P&gt;&lt;P&gt;Thank you in advance for your help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 07 Jan 2021 08:57:22 GMT</pubDate>
    <dc:creator>rdte</dc:creator>
    <dc:date>2021-01-07T08:57:22Z</dc:date>
    <item>
      <title>LPC2468FBD208 revB failed ICT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1208152#M43476</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can someone help me to solve the problem I encountered during ICT ? Using rev.B of this device zener diode voltage is pulled low but when using rev.D, ICT passed. I checked the errata sheet and cannot find any information related to this.&lt;/P&gt;&lt;P&gt;Additional question, does rev.B and rev.D have different device ID ?&lt;/P&gt;&lt;P&gt;Thank you in advance for your help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 08:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1208152#M43476</guid>
      <dc:creator>rdte</dc:creator>
      <dc:date>2021-01-07T08:57:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2468FBD208 revB failed ICT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1208170#M43477</link>
      <description>&lt;P&gt;Hi, Maria,&lt;/P&gt;
&lt;P&gt;Can you tell us what the ICT means? regarding the zener diode voltage, I have checked the UM of lpc24xx, I do not find out any zener diode, do you use external zener diode?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 09:29:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1208170#M43477</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-01-07T09:29:39Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2468FBD208 revB failed ICT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1208176#M43478</link>
      <description>&lt;P&gt;ICT is in-circuit testing. Yes, external zener diode.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 09:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1208176#M43478</guid>
      <dc:creator>rdte</dc:creator>
      <dc:date>2021-01-07T09:36:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2468FBD208 revB failed ICT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1208784#M43491</link>
      <description>&lt;P&gt;Hi, Maria,&lt;/P&gt;
&lt;P&gt;For the zener diode, generally it' cathode is connected to a serial resistor, then a power supply, it's anode is connected to GND, in the condition, the zener diode can output a constant voltage. How do you connect the zener diode to LPC2468?&lt;/P&gt;
&lt;P&gt;Regarding ICT, do you use boundary scan tools to test the internal circuit?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun rong&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 08:08:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1208784#M43491</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-01-08T08:08:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2468FBD208 revB failed ICT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1211554#M43568</link>
      <description>&lt;P&gt;Hi xinagjun,&lt;/P&gt;&lt;P&gt;The zener diode is connected to a serial resistor. Zener is used to protect pin 18 of LPC2468FBD208, in case a high voltage (transient) is present at P1-10 and P1-9. Zener is connected to pin 18.&lt;/P&gt;&lt;P&gt;On boundary scan. yes, we use boundary scan tools to test the internal circuit but fails with an error in the internal ID code.&lt;/P&gt;&lt;P&gt;Thank you in advance for your support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Maria&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 07:20:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1211554#M43568</guid>
      <dc:creator>rdte</dc:creator>
      <dc:date>2021-01-14T07:20:53Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2468FBD208 revB failed ICT</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1217566#M43644</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that you connect the GPIO pin to the cathode pin of zener node, in the case, the GPIO pin voltage is clamped to a fixed voltage, if the ICT tools set the GPIO pin in input mode, no problem. But if the ICT tools set the GPIO pin in output mode, there is issue.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 03:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2468FBD208-revB-failed-ICT/m-p/1217566#M43644</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-01-20T03:21:20Z</dc:date>
    </item>
  </channel>
</rss>