<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: /dev/ttyACM0 not created on ubuntu 20.04 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/dev-ttyACM0-not-created-on-ubuntu-20-04/m-p/1206743#M43453</link>
    <description>&lt;P&gt;The tty device is not created until you have loaded the LPCScrypt software into the device. It is initially enumerated as a DFU device, which LPCScrypt uses to load its firmware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, what you are seeing is normal. Just run LPCScrypt.&lt;/P&gt;</description>
    <pubDate>Tue, 05 Jan 2021 09:16:08 GMT</pubDate>
    <dc:creator>converse</dc:creator>
    <dc:date>2021-01-05T09:16:08Z</dc:date>
    <item>
      <title>/dev/ttyACM0 not created on ubuntu 20.04</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/dev-ttyACM0-not-created-on-ubuntu-20-04/m-p/1206626#M43452</link>
      <description>&lt;P&gt;Hi, when I set an LPC1837 into programming mode, I can see it via lsusb:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;matthias@i9:/lib/udev/rules.d$ lsusb
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 001 Device 003: ID 045e:07a5 Microsoft Corp. Wireless Receiver 1461C
Bus 001 Device 007: ID 1fc9:000c NXP Semiconductors LPC
Bus 001 Device 004: ID 0a12:0001 Cambridge Silicon Radio, Ltd Bluetooth Dongle (HCI mode)
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But the /dev/ttyACM0 device, which is required for LPCScrypt to program the µC, is not created.&amp;nbsp;&lt;BR /&gt;I'm sure that someone else already solved this problem, please post your solution!&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;BR /&gt;Matthias&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jan 2021 08:15:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/dev-ttyACM0-not-created-on-ubuntu-20-04/m-p/1206626#M43452</guid>
      <dc:creator>MatthiasBiel</dc:creator>
      <dc:date>2021-01-05T08:15:11Z</dc:date>
    </item>
    <item>
      <title>Re: /dev/ttyACM0 not created on ubuntu 20.04</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/dev-ttyACM0-not-created-on-ubuntu-20-04/m-p/1206743#M43453</link>
      <description>&lt;P&gt;The tty device is not created until you have loaded the LPCScrypt software into the device. It is initially enumerated as a DFU device, which LPCScrypt uses to load its firmware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, what you are seeing is normal. Just run LPCScrypt.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jan 2021 09:16:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/dev-ttyACM0-not-created-on-ubuntu-20-04/m-p/1206743#M43453</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-01-05T09:16:08Z</dc:date>
    </item>
    <item>
      <title>Re: /dev/ttyACM0 not created on ubuntu 20.04</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/dev-ttyACM0-not-created-on-ubuntu-20-04/m-p/1206803#M43455</link>
      <description>&lt;P&gt;So just another case of RTFM &lt;LI-EMOJI id="lia_winking-face" title=":winking_face:"&gt;&lt;/LI-EMOJI&gt; Thank you for putting me on the right track!&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jan 2021 10:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/dev-ttyACM0-not-created-on-ubuntu-20-04/m-p/1206803#M43455</guid>
      <dc:creator>MatthiasBiel</dc:creator>
      <dc:date>2021-01-05T10:37:02Z</dc:date>
    </item>
  </channel>
</rss>