<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUSB Mass Storage LPC1768 SDCard</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-LPC1768-SDCard/m-p/1206204#M43441</link>
    <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am working with LPC1768 and now i need to use this device as USB Mass Storage, connect it to a computer and see files stored in a SD card with SPI interface. I am new using the USB Interface for this type of application, then first of all, is it possible to do that? what i must read or there are some examples to check? I am attentive to your comments.&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;</description>
    <pubDate>Mon, 04 Jan 2021 16:16:42 GMT</pubDate>
    <dc:creator>contr2889</dc:creator>
    <dc:date>2021-01-04T16:16:42Z</dc:date>
    <item>
      <title>USB Mass Storage LPC1768 SDCard</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-LPC1768-SDCard/m-p/1206204#M43441</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am working with LPC1768 and now i need to use this device as USB Mass Storage, connect it to a computer and see files stored in a SD card with SPI interface. I am new using the USB Interface for this type of application, then first of all, is it possible to do that? what i must read or there are some examples to check? I am attentive to your comments.&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jan 2021 16:16:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-LPC1768-SDCard/m-p/1206204#M43441</guid>
      <dc:creator>contr2889</dc:creator>
      <dc:date>2021-01-04T16:16:42Z</dc:date>
    </item>
    <item>
      <title>Re: USB Mass Storage LPC1768 SDCard</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-LPC1768-SDCard/m-p/1207056#M43461</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the USB mass storage device example you can take a look to the &lt;A href="https://www.keil.com/support/man/docs/mcb1700/mcb1700_examples.htm" target="_blank"&gt;Keil MDK software package&lt;/A&gt; for the MCB1700 Board which includes an example of this.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="image.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/134038i1EE96F18A22276A0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;Also, I recommend you to check &lt;A href="https://www.nxp.com/docs/en/application-note/AN11070.zip" target="_blank"&gt;AN11070&lt;/A&gt; that describes how to use the SPI/SSP interface on the LPC1700 family MCU to access Secure Digital Card (SDC) or Multi Media Card (MMC).&lt;/P&gt;
&lt;P&gt;Hope it helps!&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jan 2021 19:24:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-LPC1768-SDCard/m-p/1207056#M43461</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-01-05T19:24:26Z</dc:date>
    </item>
  </channel>
</rss>