<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic sha-512 generation with lpc55s69 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/sha-512-generation-with-lpc55s69/m-p/1205542#M43435</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using LPC55s69 in an access control application development. The device has hardware accelerated sha-256 generation, which I use. However, now in addition I need sha-512 hashes. How can I do that with lpc55s69, preferably with HW support (e.g. repeated application and extension of sha 256 hashes)? A code snipped would be appreciated! If the only solution is software, is there a library, I can use (I am using MCUXpresso as IDE)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for any help with this,&lt;/P&gt;&lt;P&gt;Steffen&lt;/P&gt;</description>
    <pubDate>Fri, 01 Jan 2021 12:15:37 GMT</pubDate>
    <dc:creator>steffen_norbert</dc:creator>
    <dc:date>2021-01-01T12:15:37Z</dc:date>
    <item>
      <title>sha-512 generation with lpc55s69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/sha-512-generation-with-lpc55s69/m-p/1205542#M43435</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using LPC55s69 in an access control application development. The device has hardware accelerated sha-256 generation, which I use. However, now in addition I need sha-512 hashes. How can I do that with lpc55s69, preferably with HW support (e.g. repeated application and extension of sha 256 hashes)? A code snipped would be appreciated! If the only solution is software, is there a library, I can use (I am using MCUXpresso as IDE)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for any help with this,&lt;/P&gt;&lt;P&gt;Steffen&lt;/P&gt;</description>
      <pubDate>Fri, 01 Jan 2021 12:15:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/sha-512-generation-with-lpc55s69/m-p/1205542#M43435</guid>
      <dc:creator>steffen_norbert</dc:creator>
      <dc:date>2021-01-01T12:15:37Z</dc:date>
    </item>
    <item>
      <title>Re: sha-512 generation with lpc55s69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/sha-512-generation-with-lpc55s69/m-p/1206408#M43448</link>
      <description>&lt;P&gt;Hi, Steffen,&lt;/P&gt;
&lt;P&gt;For LPC55Sxx family, the on-chip hash module only supports SHA-1 and SHA-2 with 256-bit digest (SHA-256), it does not support SHA-512.&lt;/P&gt;
&lt;P&gt;But the software in SDK package supports SHA-512. In SDK package, there is _mbed-crypto_selftest example, you can refer to it.&lt;/P&gt;
&lt;P&gt;You can download SDK package from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1609816423641.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133877i886FED3F24289D55/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1609816423641.png" alt="xiangjun_rong_0-1609816423641.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1609816423641.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jan 2021 03:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/sha-512-generation-with-lpc55s69/m-p/1206408#M43448</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-01-05T03:16:51Z</dc:date>
    </item>
  </channel>
</rss>