<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC5410x : DMA RELOAD 'self'?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-DMA-RELOAD-self/m-p/1204604#M43383</link>
    <description>&lt;P&gt;When setting up a DMA channel descriptor, is there any reason that you cannot use the 'next' field of the descriptor to point back to itself so that the descriptor reloads itself every time it is exhausted? Is this the recommended way to achieve this type of 'self reloading' behavior?&lt;/P&gt;&lt;P&gt;For example:&lt;/P&gt;&lt;DIV&gt;&lt;PRE&gt;&lt;SPAN&gt;DMA_CHDESC_T dmaDesc;&lt;BR /&gt;...&lt;BR /&gt;&lt;/SPAN&gt;dmaDesc.next = DMA_ADDR(&amp;amp;dmaDesc);&lt;/PRE&gt;&lt;/DIV&gt;</description>
    <pubDate>Mon, 28 Dec 2020 18:05:59 GMT</pubDate>
    <dc:creator>BTaylor</dc:creator>
    <dc:date>2020-12-28T18:05:59Z</dc:date>
    <item>
      <title>LPC5410x : DMA RELOAD 'self'?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-DMA-RELOAD-self/m-p/1204604#M43383</link>
      <description>&lt;P&gt;When setting up a DMA channel descriptor, is there any reason that you cannot use the 'next' field of the descriptor to point back to itself so that the descriptor reloads itself every time it is exhausted? Is this the recommended way to achieve this type of 'self reloading' behavior?&lt;/P&gt;&lt;P&gt;For example:&lt;/P&gt;&lt;DIV&gt;&lt;PRE&gt;&lt;SPAN&gt;DMA_CHDESC_T dmaDesc;&lt;BR /&gt;...&lt;BR /&gt;&lt;/SPAN&gt;dmaDesc.next = DMA_ADDR(&amp;amp;dmaDesc);&lt;/PRE&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 28 Dec 2020 18:05:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-DMA-RELOAD-self/m-p/1204604#M43383</guid>
      <dc:creator>BTaylor</dc:creator>
      <dc:date>2020-12-28T18:05:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5410x : DMA RELOAD 'self'?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-DMA-RELOAD-self/m-p/1205321#M43406</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/33434"&gt;@BTaylor&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I think a better approach for this is using a ping-pong transfer. For more information about this check the &lt;EM&gt;12.5.4 &lt;/EM&gt;&amp;nbsp;section of the reference manual and the following community &lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/DMA-Ping-Pong-application/ta-p/1120977" target="_self"&gt;post&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 22:03:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-DMA-RELOAD-self/m-p/1205321#M43406</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-12-30T22:03:57Z</dc:date>
    </item>
  </channel>
</rss>