<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to transmit &amp;amp; receive data via USB_High speed(U2) &amp;amp; USB_Full speedU3 PORTS in LPC546 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1204223#M43369</link>
    <description>&lt;P&gt;When you use on-board USB debug, VCOM function provided by the on-board Debug Probe which is not available when using an external debug probe. That's why you can send out data to docklight through it.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For on board FSUSB and HSUSB ports, user needs to refer sdk demo&amp;nbsp;usb_device_cdc_vcom set the related USB interface as VCOM (CDC class)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 25 Dec 2020 03:08:35 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2020-12-25T03:08:35Z</dc:date>
    <item>
      <title>How to transmit &amp; receive data via USB_High speed(U2) &amp; USB_Full speedU3 PORTS in LPC54628(OM13098)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1202804#M43333</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am Karthikeyan J&lt;/P&gt;&lt;P&gt;How to transmit and receive data via USB_High speed(U2) &amp;amp; USB_Full speed(U3) PORTS in LPC54628(OM13098).&lt;/P&gt;&lt;P&gt;Through Register level programming.&lt;/P&gt;&lt;P&gt;i wanted to transmit and receive data... i used to see it through&amp;nbsp; Docklight.&lt;/P&gt;&lt;P&gt;i done a register level programming and i dumped it through Debug_USB,&lt;/P&gt;&lt;P&gt;but when i removed it and connect it to USB_High speed(u2) port means it was showing an error that (the communication port could not be opened. Device not available).&lt;/P&gt;&lt;P&gt;even i connected two USB cables for both usb_debug port and usb_high speed port, but the usb_High speed port is not considered at all.&lt;/P&gt;&lt;P&gt;so my question is , How to enable this USB_high speed port and how to transmit and receive data through it.&lt;/P&gt;&lt;P&gt;How to program it.&lt;/P&gt;&lt;P&gt;with regards&lt;/P&gt;&lt;P&gt;karthikeyan.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 06:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1202804#M43333</guid>
      <dc:creator>Karthikeyan_J</dc:creator>
      <dc:date>2020-12-22T06:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: How to transmit &amp; receive data via USB_High speed(U2) &amp; USB_Full speedU3 PORTS in LPC546</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1204087#M43364</link>
      <description>&lt;P&gt;you want to send out data via USB1 to docklight but failed.&lt;/P&gt;
&lt;P&gt;Do you config USB1 CDC?&lt;/P&gt;
&lt;P&gt;when you connect two USB (one for debug, the other for USB1), can your docklight recognize both of them?&lt;/P&gt;
&lt;P&gt;Please verify when two USBs connected, make sure the docklight received data are from USB1.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 09:49:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1204087#M43364</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-12-24T09:49:07Z</dc:date>
    </item>
    <item>
      <title>Re: How to transmit &amp; receive data via USB_High speed(U2) &amp; USB_Full speedU3 PORTS in LPC546</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1204124#M43366</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for your reply,&lt;/P&gt;&lt;P&gt;sending or receiving via USB1 to docklight is failed.&lt;/P&gt;&lt;P&gt;no i didn't use&amp;nbsp;&lt;SPAN&gt;config USB1 CDC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;when i am&amp;nbsp; connecting two USB (one for debug, the other for USB1),only the debug port is get recognized, but the USB1 port is not get recognized.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanking you,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Karthikeyan.J&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 12:33:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1204124#M43366</guid>
      <dc:creator>Karthikeyan_J</dc:creator>
      <dc:date>2020-12-24T12:33:21Z</dc:date>
    </item>
    <item>
      <title>Re: How to transmit &amp; receive data via USB_High speed(U2) &amp; USB_Full speedU3 PORTS in LPC546</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1204223#M43369</link>
      <description>&lt;P&gt;When you use on-board USB debug, VCOM function provided by the on-board Debug Probe which is not available when using an external debug probe. That's why you can send out data to docklight through it.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For on board FSUSB and HSUSB ports, user needs to refer sdk demo&amp;nbsp;usb_device_cdc_vcom set the related USB interface as VCOM (CDC class)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Dec 2020 03:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1204223#M43369</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-12-25T03:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: How to transmit &amp; receive data via USB_High speed(U2) &amp; USB_Full speedU3 PORTS in LPC546</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1204321#M43371</link>
      <description>&lt;P&gt;Hi Zhang,&lt;/P&gt;&lt;P&gt;I tried the program&amp;nbsp;&lt;SPAN&gt;usb_device_cdc_vcom, the code runs successfully, but the device manager could not able recognize the port and i attached the error messages, please do send me the solution as soon as possible.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;suggest a driver to install.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanking you,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Karthikeyan.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 26 Dec 2020 06:24:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1204321#M43371</guid>
      <dc:creator>Karthikeyan_J</dc:creator>
      <dc:date>2020-12-26T06:24:08Z</dc:date>
    </item>
    <item>
      <title>Re: How to transmit &amp; receive data via USB_High speed(U2) &amp; USB_Full speedU3 PORTS in LPC546</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1204416#M43376</link>
      <description>&lt;P&gt;I ever tested this demo. I can confirm there is no issue on it.&lt;/P&gt;
&lt;P&gt;On my 64bit win10，windows can find cdc driver automatically.&lt;/P&gt;
&lt;P&gt;On my 32bit xp, need to install driver from inf folder inside the demo code.&lt;/P&gt;
&lt;P&gt;So If your windows can't recognize usb device, install driver from inf folder manually.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Mon, 28 Dec 2020 04:19:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-transmit-amp-receive-data-via-USB-High-speed-U2-amp-USB/m-p/1204416#M43376</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-12-28T04:19:31Z</dc:date>
    </item>
  </channel>
</rss>