<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC55xx with external clock</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-with-external-clock/m-p/1203232#M43342</link>
    <description>&lt;P&gt;The datasheet for the LPC55S6x states that an external clock can be used on the XTAL32M_P pin if the clock is a square wave from 0V to 850mV.&amp;nbsp; Can someone elaborate on this? What is the tolerance of "0" and "850mV"?&amp;nbsp; Is a DC offset acceptable as long as the amplitude is 850mVpp? Is 850mV the absolute maximum for the the pin?&lt;/P&gt;&lt;P&gt;Previous LPC parts allowed an external oscillator to be capacitor divided and driven into the XTALIN pin, but that process will not guarantee a 0-850mV signal from a 3.3V oscillator (there will be some DC offset).&amp;nbsp; Without a little more information (or a recommended circuit) it is near impossible to design a robust system.&lt;/P&gt;</description>
    <pubDate>Tue, 22 Dec 2020 21:28:28 GMT</pubDate>
    <dc:creator>otsl</dc:creator>
    <dc:date>2020-12-22T21:28:28Z</dc:date>
    <item>
      <title>LPC55xx with external clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-with-external-clock/m-p/1203232#M43342</link>
      <description>&lt;P&gt;The datasheet for the LPC55S6x states that an external clock can be used on the XTAL32M_P pin if the clock is a square wave from 0V to 850mV.&amp;nbsp; Can someone elaborate on this? What is the tolerance of "0" and "850mV"?&amp;nbsp; Is a DC offset acceptable as long as the amplitude is 850mVpp? Is 850mV the absolute maximum for the the pin?&lt;/P&gt;&lt;P&gt;Previous LPC parts allowed an external oscillator to be capacitor divided and driven into the XTALIN pin, but that process will not guarantee a 0-850mV signal from a 3.3V oscillator (there will be some DC offset).&amp;nbsp; Without a little more information (or a recommended circuit) it is near impossible to design a robust system.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 21:28:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-with-external-clock/m-p/1203232#M43342</guid>
      <dc:creator>otsl</dc:creator>
      <dc:date>2020-12-22T21:28:28Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx with external clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-with-external-clock/m-p/1203634#M43351</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;DC offset is not acceptable as long as the amplitude is 850mVpp.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;850mV is the absolute maximum for the the pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;this pin absolute input range is 0-850mV.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Fri, 25 Dec 2020 01:25:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-with-external-clock/m-p/1203634#M43351</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-12-25T01:25:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx with external clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-with-external-clock/m-p/1205257#M43402</link>
      <description>&lt;P&gt;Thank you Jun. Can you also provide the minimum amplitude that will reliably be detected?&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 11:57:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-with-external-clock/m-p/1205257#M43402</guid>
      <dc:creator>otsl</dc:creator>
      <dc:date>2020-12-30T11:57:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx with external clock</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-with-external-clock/m-p/1205586#M43416</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;We don't have this&amp;nbsp;&lt;SPAN&gt;minimum amplitude data.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;But based on practice, I suggest you make sure the amplitude over 100mV.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 02 Jan 2021 08:21:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-with-external-clock/m-p/1205586#M43416</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-01-02T08:21:35Z</dc:date>
    </item>
  </channel>
</rss>