<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Failed on connect: Ep(01). Target marked as not debuggable.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/1201919#M43308</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180834"&gt;@VictorDiaconu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing well!&lt;/P&gt;
&lt;P&gt;So, If you try to trigger the mass erase once again with&amp;nbsp; J10 installed or&amp;nbsp; releasing ISP button after reset the process fails again?&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;&lt;FONT color="#333333"&gt;From my experience, you can set the MCU into ISP mode ( by installing J10 when the board&amp;nbsp; or releasing ISP button after refer ) and then trigger a mass erase. However you do not need to set the MCU into ISP mode to trigger a mass erase. Having the MCU into ISP mode, helps to recover debugger connection in some cases,&amp;nbsp; see &lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Regaining-debug-access-to-target-MCU/m-p/473923" target="_self"&gt;Regainning debug access to target MCU&lt;/A&gt;.&amp;nbsp; After&amp;nbsp;&amp;nbsp; the mass erase was succesful, you may want to uninstall the J10 to trigger a debug session.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;Also, to&amp;nbsp; recover the MCU , we can try by using Flash magic Tool&amp;nbsp; , J-link commander or even an external debug probe, if required we can check them.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;</description>
    <pubDate>Fri, 18 Dec 2020 18:21:41 GMT</pubDate>
    <dc:creator>diego_charles</dc:creator>
    <dc:date>2020-12-18T18:21:41Z</dc:date>
    <item>
      <title>Failed on connect: Ep(01). Target marked as not debuggable.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/1201321#M43299</link>
      <description>&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I have now a problem. Pleas help me. I can't start the Debug session on LPCXpresso 55s28.&lt;/P&gt;&lt;P&gt;Early it work fine, but after that I done a mistake by Flash Erase and now debug session doesn't start anymore.&lt;/P&gt;&lt;P&gt;I wanted to Erase the Flash Memory. But I forgot to set jumper J10.&lt;/P&gt;&lt;P&gt;I have done:&lt;/P&gt;&lt;P&gt;1. Press reset button.&lt;BR /&gt;2. Open Gui Flash Tool&lt;BR /&gt;3. at Erase Tab I selected Mass erase and pusch the Run... Button.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hier are the errors :&lt;/P&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.2 (Sep 22 2020 13:23:35 - crt_emu_cm_redlink build 19)&lt;BR /&gt;Found chip XML file in D:/EMV_SW_NG/EMV_SW_NG_VoxioA/Debug\LPC55S28.xml&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;Probe Firmware: LPC-LINK2 CMSIS-DAP V5.224 (NXP Semiconductors)&lt;BR /&gt;Serial Number: ORAWCQCQ&lt;BR /&gt;VID:PID: 1FC9:0090&lt;BR /&gt;USB Path: \\?\hid#vid_1fc9&amp;amp;pid_0090&amp;amp;mi_00#9&amp;amp;575fa1&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;Using memory from core 0 after searching for a good core&lt;BR /&gt;On debug connection - use system reset, stalling when 0x50000040 is accessed&lt;BR /&gt;Retask read watchpoint 1 at 0x50000040 to use for boot ROM stall&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;failed to use debug bus when CPU is stalled - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;Debug bus check after stop (MemAP 0x84770001) FAILS - Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;Failed on connect: Ep(01). Target marked as not debuggable.&lt;BR /&gt;Connected&amp;amp;Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000D21. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Last stub error 0: OK&lt;BR /&gt;Last sticky error: 0x10 POWER AIndex: 0&lt;BR /&gt;Debug bus selected: MemAp 0&lt;BR /&gt;DAP Speed test unexecuted or failed&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Enabled.&lt;BR /&gt;error closing down debug session - Nn(05). Wire ACK Fault in DAP access&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Debug Errors.JPG" style="width: 973px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/132982i072136F012E72969/image-size/large?v=v2&amp;amp;px=999" role="button" title="Debug Errors.JPG" alt="Debug Errors.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Debug Errors.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 15:50:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/1201321#M43299</guid>
      <dc:creator>VictorDiaconu</dc:creator>
      <dc:date>2020-12-17T15:50:41Z</dc:date>
    </item>
    <item>
      <title>Re: Failed on connect: Ep(01). Target marked as not debuggable.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/1201919#M43308</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180834"&gt;@VictorDiaconu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing well!&lt;/P&gt;
&lt;P&gt;So, If you try to trigger the mass erase once again with&amp;nbsp; J10 installed or&amp;nbsp; releasing ISP button after reset the process fails again?&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;&lt;FONT color="#333333"&gt;From my experience, you can set the MCU into ISP mode ( by installing J10 when the board&amp;nbsp; or releasing ISP button after refer ) and then trigger a mass erase. However you do not need to set the MCU into ISP mode to trigger a mass erase. Having the MCU into ISP mode, helps to recover debugger connection in some cases,&amp;nbsp; see &lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Regaining-debug-access-to-target-MCU/m-p/473923" target="_self"&gt;Regainning debug access to target MCU&lt;/A&gt;.&amp;nbsp; After&amp;nbsp;&amp;nbsp; the mass erase was succesful, you may want to uninstall the J10 to trigger a debug session.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;Also, to&amp;nbsp; recover the MCU , we can try by using Flash magic Tool&amp;nbsp; , J-link commander or even an external debug probe, if required we can check them.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;</description>
      <pubDate>Fri, 18 Dec 2020 18:21:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/1201919#M43308</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2020-12-18T18:21:41Z</dc:date>
    </item>
    <item>
      <title>Re: Failed on connect: Ep(01). Target marked as not debuggable.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/1205823#M43427</link>
      <description>&lt;P&gt;Hi &lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/89833" target="_self"&gt;&lt;SPAN class=""&gt;diego_charles&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, I done&amp;nbsp;the mass erase&amp;nbsp;many time, but this did not help me. After that I remember that early I have change the Debug Configuration Settings. And I setted them all to default. And now it work very well.&lt;/P&gt;&lt;P&gt;It is stranger for me, erally with another Debug Configuration i can debug the Code. And after a short way to erase the chip (three step to erase the chip) I must first to set the Debug Configuration back to make all work properly.&lt;/P&gt;&lt;P&gt;Finally Debug Configuration are not important for me. More important that I can debug again.&lt;/P&gt;&lt;P&gt;Thank you for your help&amp;nbsp;&lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/89833" target="_self"&gt;diego_charles&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Victor Diaconu&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jan 2021 06:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/1205823#M43427</guid>
      <dc:creator>VictorDiaconu</dc:creator>
      <dc:date>2021-01-04T06:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: Failed on connect: Ep(01). Target marked as not debuggable.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/1206199#M43440</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180834"&gt;@VictorDiaconu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your reply as well,&lt;/P&gt;
&lt;P&gt;Happy new year,&lt;/P&gt;
&lt;P&gt;Diego.&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jan 2021 15:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/1206199#M43440</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2021-01-04T15:43:53Z</dc:date>
    </item>
  </channel>
</rss>