<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC4078 FLASHCFG settings. in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4078-FLASHCFG-settings/m-p/1201765#M43305</link>
    <description>&lt;P&gt;Customer operated at 96 MHz CPU frequency with FLASHCFG register&amp;nbsp;reset value 0x3(0011 Flash accesses use 4 CPU clocks. Use for up to 80 MHz CPU clock with power boost off (see Section 3.12.6).) and PBOOST register reset value 0x3(11 : Boost is on, operation up to 120 MHz is supported.).&lt;/P&gt;
&lt;P&gt;Is this correct and safe settings?Thanks.&lt;/P&gt;</description>
    <pubDate>Fri, 18 Dec 2020 10:26:29 GMT</pubDate>
    <dc:creator>yangyu</dc:creator>
    <dc:date>2020-12-18T10:26:29Z</dc:date>
    <item>
      <title>LPC4078 FLASHCFG settings.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4078-FLASHCFG-settings/m-p/1201765#M43305</link>
      <description>&lt;P&gt;Customer operated at 96 MHz CPU frequency with FLASHCFG register&amp;nbsp;reset value 0x3(0011 Flash accesses use 4 CPU clocks. Use for up to 80 MHz CPU clock with power boost off (see Section 3.12.6).) and PBOOST register reset value 0x3(11 : Boost is on, operation up to 120 MHz is supported.).&lt;/P&gt;
&lt;P&gt;Is this correct and safe settings?Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Dec 2020 10:26:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4078-FLASHCFG-settings/m-p/1201765#M43305</guid>
      <dc:creator>yangyu</dc:creator>
      <dc:date>2020-12-18T10:26:29Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4078 FLASHCFG settings.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4078-FLASHCFG-settings/m-p/1202124#M43312</link>
      <description>&lt;P&gt;Hi, YuYang,&lt;/P&gt;
&lt;P&gt;As the following figure, if you use 96MHz CPU clock, you can set the FLASHTIM bits as 0x100(5 cpu clocks with power boost off).&lt;/P&gt;
&lt;P&gt;Power boost off can be set up as:&lt;/P&gt;
&lt;P&gt;PBOOST=0x00;&lt;/P&gt;
&lt;P&gt;I copy it here:&lt;/P&gt;
&lt;P&gt;"0100 Flash accesses use 5 CPU clocks. Use for up to 100 MHz CPU clock with power boost off (see Section 3.12.6)."&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1608516052910.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133142iBF67883E6CF21B6A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1608516052910.png" alt="xiangjun_rong_0-1608516052910.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Power boost control reg&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_1-1608516519422.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133146i78E6E2CDC3E57F72/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_1-1608516519422.png" alt="xiangjun_rong_1-1608516519422.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 02:09:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4078-FLASHCFG-settings/m-p/1202124#M43312</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-12-21T02:09:28Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4078 FLASHCFG settings.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4078-FLASHCFG-settings/m-p/1202149#M43313</link>
      <description>&lt;P&gt;Hi Xiangjun,&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;In other word,with default reset value of FLASHTIM&amp;amp;Boost&amp;nbsp;the cpu runs at 96MHz is unsafe?&lt;/P&gt;
&lt;P&gt;In general,the designers don't notice these registers settings and just use the default value.Any official documents or sample codes to remind users?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 02:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4078-FLASHCFG-settings/m-p/1202149#M43313</guid>
      <dc:creator>yangyu</dc:creator>
      <dc:date>2020-12-21T02:41:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4078 FLASHCFG settings.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4078-FLASHCFG-settings/m-p/1202334#M43315</link>
      <description>&lt;P&gt;Hi, Yuyang,&lt;/P&gt;
&lt;P&gt;Firstly, I do not think there is any documentation to remind user of the FLASHTIM&amp;amp;Boost registers.&lt;/P&gt;
&lt;P&gt;Regarding your question whether it is safe to use the default FLASHTIM(3) and PBOOST(3) when the LPC4078 runs in 96MHz, I can not say it is safe or not.&lt;/P&gt;
&lt;P&gt;I suggest you do a full temperature range test, if the chip runs okay in full temperature range especially in high temperature, it is okay.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 08:04:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4078-FLASHCFG-settings/m-p/1202334#M43315</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-12-21T08:04:04Z</dc:date>
    </item>
  </channel>
</rss>