<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC 55s69 - Host USB CDC example is not working</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-55s69-Host-USB-CDC-example-is-not-working/m-p/1201031#M43291</link>
    <description>&lt;P&gt;There is an excellent article by Jennie Zhang :&amp;nbsp;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Using-ConfigTool-to-create-USB-Project-From-Start/ta-p/1103294" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Using-ConfigTool-to-create-USB-Project-From-Start/ta-p/1103294&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also have a look at some stuff I did to print with USB CDC, this is however just printing to teraterm on a PC, and NOT processing stuff received from the PC&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/USB-DeviceCdcAcmSend-value-of-class-handle-class-handle-t-on/m-p/1152780#M42218" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/USB-DeviceCdcAcmSend-value-of-class-handle-class-handle-t-on/m-p/1152780#M42218&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 17 Dec 2020 07:28:25 GMT</pubDate>
    <dc:creator>gertvb</dc:creator>
    <dc:date>2020-12-17T07:28:25Z</dc:date>
    <item>
      <title>LPC 55s69 - Host USB CDC example is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-55s69-Host-USB-CDC-example-is-not-working/m-p/1200154#M43273</link>
      <description>&lt;P&gt;I import the SDK 2.0 Host USB CDC example for testing its not working as it is. I disable the serial port then try its working and detect the USB CDC device but I am not able to understand how to USB receive INTR or USB receive polling.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, Can you help me for simple Rx and Tx communication API or example code?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Dec 2020 07:10:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-55s69-Host-USB-CDC-example-is-not-working/m-p/1200154#M43273</guid>
      <dc:creator>pateln948</dc:creator>
      <dc:date>2020-12-16T07:10:10Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 55s69 - Host USB CDC example is not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-55s69-Host-USB-CDC-example-is-not-working/m-p/1201031#M43291</link>
      <description>&lt;P&gt;There is an excellent article by Jennie Zhang :&amp;nbsp;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Using-ConfigTool-to-create-USB-Project-From-Start/ta-p/1103294" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Using-ConfigTool-to-create-USB-Project-From-Start/ta-p/1103294&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also have a look at some stuff I did to print with USB CDC, this is however just printing to teraterm on a PC, and NOT processing stuff received from the PC&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/USB-DeviceCdcAcmSend-value-of-class-handle-class-handle-t-on/m-p/1152780#M42218" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/USB-DeviceCdcAcmSend-value-of-class-handle-class-handle-t-on/m-p/1152780#M42218&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 07:28:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-55s69-Host-USB-CDC-example-is-not-working/m-p/1201031#M43291</guid>
      <dc:creator>gertvb</dc:creator>
      <dc:date>2020-12-17T07:28:25Z</dc:date>
    </item>
  </channel>
</rss>