<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC5410x : DMA Burst Transfer</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-DMA-Burst-Transfer/m-p/1200629#M43285</link>
    <description>&lt;P&gt;What is the difference between configuring a DMA channel with TRIGBURST = 0 (single transfer) and configuring the channel with TRIGBURST = 1 (burst transfer) and BURSTPOWER = 0 (burst size 1)? In other words, what is the difference between configuring a single transfer and configuring a burst transfer of size 1?&lt;/P&gt;&lt;P&gt;Also...the LPC5410x user manual indicates that that TRIGBURST "[s]elects whether hardware triggers cause a single or burst transfer". Is TRIGBURST really only applicable when hardware triggering is used or is it also applicable when software triggering is used?&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 16 Dec 2020 19:31:00 GMT</pubDate>
    <dc:creator>BTaylor</dc:creator>
    <dc:date>2020-12-16T19:31:00Z</dc:date>
    <item>
      <title>LPC5410x : DMA Burst Transfer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-DMA-Burst-Transfer/m-p/1200629#M43285</link>
      <description>&lt;P&gt;What is the difference between configuring a DMA channel with TRIGBURST = 0 (single transfer) and configuring the channel with TRIGBURST = 1 (burst transfer) and BURSTPOWER = 0 (burst size 1)? In other words, what is the difference between configuring a single transfer and configuring a burst transfer of size 1?&lt;/P&gt;&lt;P&gt;Also...the LPC5410x user manual indicates that that TRIGBURST "[s]elects whether hardware triggers cause a single or burst transfer". Is TRIGBURST really only applicable when hardware triggering is used or is it also applicable when software triggering is used?&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Dec 2020 19:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-DMA-Burst-Transfer/m-p/1200629#M43285</guid>
      <dc:creator>BTaylor</dc:creator>
      <dc:date>2020-12-16T19:31:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5410x : DMA Burst Transfer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-DMA-Burst-Transfer/m-p/1201086#M43293</link>
      <description>&lt;P&gt;Hi, Brandon,&lt;/P&gt;
&lt;P&gt;I think the two configurations are the same that configures a DMA channel with TRIGBURST = 0 (single transfer) and configure the channel with TRIGBURST = 1 (burst transfer) and BURSTPOWER = 0 (burst size 1). In the two cases, the DMA will transfer the bytes defined in WIDTH bits in Channel transfer configuration registers for each trigger.&lt;/P&gt;
&lt;P&gt;I think the burst transfer is only valid for hardware triggering.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun rong&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 08:30:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5410x-DMA-Burst-Transfer/m-p/1201086#M43293</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-12-17T08:30:32Z</dc:date>
    </item>
  </channel>
</rss>