<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB Host with LPC 4088 Pendrive configuration in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Host-with-LPC-4088-Pendrive-configuration/m-p/1199354#M43261</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;I am working on Custom board of LPC4088 in MCUexpresso enviroment .for quickstart board massstoragehost code works perfect but in my custom board i am getting device enumeration error .&lt;BR /&gt;i am geting error code As HOST_ENUMERROR_ControlError and sub error as HOST_ENUMERROR_NoDeviceDetected .The sub error code means that No device was detected, despite the USB data lines indicating the attachment of a device. it happens in HOST_STATE_Default.&lt;BR /&gt;I am using Port 0 for configuration . and in HcdIrqHandler HCD status code getting is HCD_STATUS_TRANSFER_Stall.&lt;BR /&gt;i am not able to findout why this is happening . can anyone help me on this .&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Tue, 15 Dec 2020 12:01:34 GMT</pubDate>
    <dc:creator>kshirsagaravina</dc:creator>
    <dc:date>2020-12-15T12:01:34Z</dc:date>
    <item>
      <title>USB Host with LPC 4088 Pendrive configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Host-with-LPC-4088-Pendrive-configuration/m-p/1199354#M43261</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I am working on Custom board of LPC4088 in MCUexpresso enviroment .for quickstart board massstoragehost code works perfect but in my custom board i am getting device enumeration error .&lt;BR /&gt;i am geting error code As HOST_ENUMERROR_ControlError and sub error as HOST_ENUMERROR_NoDeviceDetected .The sub error code means that No device was detected, despite the USB data lines indicating the attachment of a device. it happens in HOST_STATE_Default.&lt;BR /&gt;I am using Port 0 for configuration . and in HcdIrqHandler HCD status code getting is HCD_STATUS_TRANSFER_Stall.&lt;BR /&gt;i am not able to findout why this is happening . can anyone help me on this .&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 12:01:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Host-with-LPC-4088-Pendrive-configuration/m-p/1199354#M43261</guid>
      <dc:creator>kshirsagaravina</dc:creator>
      <dc:date>2020-12-15T12:01:34Z</dc:date>
    </item>
    <item>
      <title>Re: USB Host with LPC 4088 Pendrive configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Host-with-LPC-4088-Pendrive-configuration/m-p/1202657#M43329</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If the same software does not work with your board then it seems to be a hardware issue. Please check you are following our guidelines for full-speed USB on NXP's LPC microcontrollers.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11392.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN11392.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 23:59:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Host-with-LPC-4088-Pendrive-configuration/m-p/1202657#M43329</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-12-21T23:59:39Z</dc:date>
    </item>
  </channel>
</rss>