<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC55xx Flash Access</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Flash-Access/m-p/1199350#M43260</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to save data to the built-in Flash using LPC5514.&lt;/P&gt;&lt;P&gt;I think that the SDK "iap_flash" is mainly helpful, but I found the following description in the Note of the manual.&lt;/P&gt;&lt;P&gt;"Associated prefetches should be disabled before issuing any Flash commands."&lt;/P&gt;&lt;P&gt;I think that prefetches can be disabled by setting PREFEN, but when I check iap_flash and the device driver, I can't find the corresponding code.&lt;/P&gt;&lt;P&gt;I think I need to disable prefetches before running APIs that access flash (FLASH_Erase, FLASH_Program, etc.), is this wrong?&lt;/P&gt;&lt;P&gt;Details&lt;BR /&gt;Device: LPC5514SDK Version: 2.8.2 (released 2020-08-19)&lt;BR /&gt;Host OS: Windows&lt;BR /&gt;Toolchain: IAR Embedded Workbench for ARM&lt;/P&gt;</description>
    <pubDate>Tue, 15 Dec 2020 05:28:46 GMT</pubDate>
    <dc:creator>yamakatb</dc:creator>
    <dc:date>2020-12-15T05:28:46Z</dc:date>
    <item>
      <title>LPC55xx Flash Access</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Flash-Access/m-p/1199350#M43260</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to save data to the built-in Flash using LPC5514.&lt;/P&gt;&lt;P&gt;I think that the SDK "iap_flash" is mainly helpful, but I found the following description in the Note of the manual.&lt;/P&gt;&lt;P&gt;"Associated prefetches should be disabled before issuing any Flash commands."&lt;/P&gt;&lt;P&gt;I think that prefetches can be disabled by setting PREFEN, but when I check iap_flash and the device driver, I can't find the corresponding code.&lt;/P&gt;&lt;P&gt;I think I need to disable prefetches before running APIs that access flash (FLASH_Erase, FLASH_Program, etc.), is this wrong?&lt;/P&gt;&lt;P&gt;Details&lt;BR /&gt;Device: LPC5514SDK Version: 2.8.2 (released 2020-08-19)&lt;BR /&gt;Host OS: Windows&lt;BR /&gt;Toolchain: IAR Embedded Workbench for ARM&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 05:28:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Flash-Access/m-p/1199350#M43260</guid>
      <dc:creator>yamakatb</dc:creator>
      <dc:date>2020-12-15T05:28:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx Flash Access</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Flash-Access/m-p/1199543#M43263</link>
      <description>&lt;P&gt;Hello &lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-III lia-component-message-view-widget-author-username"&gt;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" style="color: #333f48;" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/116953" target="_self"&gt;&lt;SPAN class=""&gt;yamakatb&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;
&lt;P&gt;Yes, you are right.&lt;/P&gt;
&lt;P&gt;By default, PREFEN is disabled, so maybe the iap_flash demo missing it.&lt;/P&gt;
&lt;DIV id="tinyMceEditorAlice_Yang_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 09:18:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Flash-Access/m-p/1199543#M43263</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2020-12-15T09:18:14Z</dc:date>
    </item>
  </channel>
</rss>