<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC54S018 Drive Current in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S018-Drive-Current/m-p/1195714#M43185</link>
    <description>&lt;P&gt;I was wondering how I measure or calculate drive current to a crystal. I don't see anything in the data sheet other then calculating the correct caps and a note saying it is critical to get the drive level correct.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pg # 138 "For best results, it is very critical to select a matching crystal for the on-chip oscillator.&lt;BR /&gt;Load capacitance (CL), series resistance (RS), and drive level (DL) are important&lt;BR /&gt;parameters to consider while choosing the crystal."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The current crystal I am using for protos is running at 25mhz, 100ohm, 6pF, 150uW (300uW max). This is fairly close to what the dev kit uses. However I would like to cross this part with something more commonly available. If any special tools are required recommendations are welcomed.&lt;/P&gt;</description>
    <pubDate>Tue, 08 Dec 2020 21:45:50 GMT</pubDate>
    <dc:creator>smiller1</dc:creator>
    <dc:date>2020-12-08T21:45:50Z</dc:date>
    <item>
      <title>LPC54S018 Drive Current</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S018-Drive-Current/m-p/1195714#M43185</link>
      <description>&lt;P&gt;I was wondering how I measure or calculate drive current to a crystal. I don't see anything in the data sheet other then calculating the correct caps and a note saying it is critical to get the drive level correct.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pg # 138 "For best results, it is very critical to select a matching crystal for the on-chip oscillator.&lt;BR /&gt;Load capacitance (CL), series resistance (RS), and drive level (DL) are important&lt;BR /&gt;parameters to consider while choosing the crystal."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The current crystal I am using for protos is running at 25mhz, 100ohm, 6pF, 150uW (300uW max). This is fairly close to what the dev kit uses. However I would like to cross this part with something more commonly available. If any special tools are required recommendations are welcomed.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Dec 2020 21:45:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54S018-Drive-Current/m-p/1195714#M43185</guid>
      <dc:creator>smiller1</dc:creator>
      <dc:date>2020-12-08T21:45:50Z</dc:date>
    </item>
  </channel>
</rss>