<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC 845 DMA, new SDK functions, DMA_PrepareChannelTransfer, Trigger</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-845-DMA-new-SDK-functions-DMA-PrepareChannelTransfer-Trigger/m-p/1195515#M43182</link>
    <description>&lt;P&gt;Dear Community,&lt;/P&gt;&lt;P&gt;The LPC 845 SDK uses a DMA example which is not up to date anymore and there is the suggestion to use a newer version which uses: DMA_PrepareChannelTransfer.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;brief Prepares the DMA transfer structure.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* deprecated Do not use this function. It has been superceded by @ref DMA_PrepareChannelTransfer and, &lt;/EM&gt;&lt;EM&gt;DMA_PrepareChannelXfer.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;However, I am able to use the old functions, but I fail to run the newer version and no example was provided. Mainly the issue will be with the Trigger, due to the fact, that I do not find a proper documentation for the trigger. Does anyone made it and could provide the simplest Trigger solution.&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Tue, 08 Dec 2020 13:07:54 GMT</pubDate>
    <dc:creator>NXP_USER_11</dc:creator>
    <dc:date>2020-12-08T13:07:54Z</dc:date>
    <item>
      <title>LPC 845 DMA, new SDK functions, DMA_PrepareChannelTransfer, Trigger</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-845-DMA-new-SDK-functions-DMA-PrepareChannelTransfer-Trigger/m-p/1195515#M43182</link>
      <description>&lt;P&gt;Dear Community,&lt;/P&gt;&lt;P&gt;The LPC 845 SDK uses a DMA example which is not up to date anymore and there is the suggestion to use a newer version which uses: DMA_PrepareChannelTransfer.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;brief Prepares the DMA transfer structure.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* deprecated Do not use this function. It has been superceded by @ref DMA_PrepareChannelTransfer and, &lt;/EM&gt;&lt;EM&gt;DMA_PrepareChannelXfer.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;However, I am able to use the old functions, but I fail to run the newer version and no example was provided. Mainly the issue will be with the Trigger, due to the fact, that I do not find a proper documentation for the trigger. Does anyone made it and could provide the simplest Trigger solution.&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Tue, 08 Dec 2020 13:07:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-845-DMA-new-SDK-functions-DMA-PrepareChannelTransfer-Trigger/m-p/1195515#M43182</guid>
      <dc:creator>NXP_USER_11</dc:creator>
      <dc:date>2020-12-08T13:07:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 845 DMA, new SDK functions, DMA_PrepareChannelTransfer, Trigger</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-845-DMA-new-SDK-functions-DMA-PrepareChannelTransfer-Trigger/m-p/1199101#M43255</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The trigger can be configured with DMA_SetChannelConfig(), the structure "dma_channel_trigger_t" describes if the dma will be triggered by a low/high level, rising/falling edge or you can leave no trigger.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the trigger configuration I suggest you to check chapter 16 and chapter 14 of the LPC84x User Manual.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 18:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-845-DMA-new-SDK-functions-DMA-PrepareChannelTransfer-Trigger/m-p/1199101#M43255</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2020-12-14T18:25:19Z</dc:date>
    </item>
  </channel>
</rss>