<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Secondary Bootloader for LPC51U68 (MCUxpresso project) in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-for-LPC51U68-MCUxpresso-project/m-p/1189162#M43047</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not have any guide to port from Keil to MCUXpresso directly. However, the easiest way is to create a new project in MCUXpresso IDE and then copy the files of the application to the new project.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
    <pubDate>Wed, 25 Nov 2020 17:30:30 GMT</pubDate>
    <dc:creator>FelipeGarcia</dc:creator>
    <dc:date>2020-11-25T17:30:30Z</dc:date>
    <item>
      <title>Secondary Bootloader for LPC51U68 (MCUxpresso project)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-for-LPC51U68-MCUxpresso-project/m-p/1187437#M42990</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;we are using the LPC51U68 (LPC51U68JBD48E) for a new project on a custom board.&lt;BR /&gt;All works well and the firmware is developed on the MCUXpresso IDE&lt;BR /&gt;Now we want to use secondary bootloader in order to offer for exmple DFU via USB for our customers.&lt;BR /&gt;I know there is a manual (AN12689) to port an existing bootloader to this device, but this manual is based on the Keil IDE.&lt;/P&gt;&lt;P&gt;We are looking for a project based on the MCUXpresso IDE or at least a manual to make that secondary bootloader for the LPC51U68 working. Any help or good ideas are much appreciated.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 23 Nov 2020 11:23:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-for-LPC51U68-MCUxpresso-project/m-p/1187437#M42990</guid>
      <dc:creator>burkhard</dc:creator>
      <dc:date>2020-11-23T11:23:44Z</dc:date>
    </item>
    <item>
      <title>Re: Secondary Bootloader for LPC51U68 (MCUxpresso project)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-for-LPC51U68-MCUxpresso-project/m-p/1189162#M43047</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not have any guide to port from Keil to MCUXpresso directly. However, the easiest way is to create a new project in MCUXpresso IDE and then copy the files of the application to the new project.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 17:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Secondary-Bootloader-for-LPC51U68-MCUxpresso-project/m-p/1189162#M43047</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-11-25T17:30:30Z</dc:date>
    </item>
  </channel>
</rss>