<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC17xx USB Bootloader from Usb Memory stick</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-USB-Bootloader-from-Usb-Memory-stick/m-p/521649#M4303</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by RGB on Tue Dec 11 08:35:58 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi everybody! Is there the possibility with LPC1768 to load firmware throught an USB Memory Stick without a PC? I think that I have to implement USB MAss Storage Class in Bootloader Mode. So at reset if a GPIO is in a particular state, I enter Bootloader mode, I read the Memory stick throught File system (USB Host lite) and if there is a valid .bin file I write it into Flash. All without a PC. Freescale Kinetis has this feature. Is it possible with NXP LPC1768? Is there an application note for it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you very much&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:50:53 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:50:53Z</dc:date>
    <item>
      <title>LPC17xx USB Bootloader from Usb Memory stick</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-USB-Bootloader-from-Usb-Memory-stick/m-p/521649#M4303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by RGB on Tue Dec 11 08:35:58 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi everybody! Is there the possibility with LPC1768 to load firmware throught an USB Memory Stick without a PC? I think that I have to implement USB MAss Storage Class in Bootloader Mode. So at reset if a GPIO is in a particular state, I enter Bootloader mode, I read the Memory stick throught File system (USB Host lite) and if there is a valid .bin file I write it into Flash. All without a PC. Freescale Kinetis has this feature. Is it possible with NXP LPC1768? Is there an application note for it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you very much&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:50:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-USB-Bootloader-from-Usb-Memory-stick/m-p/521649#M4303</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:50:53Z</dc:date>
    </item>
    <item>
      <title>Re: LPC17xx USB Bootloader from Usb Memory stick</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-USB-Bootloader-from-Usb-Memory-stick/m-p/521650#M4304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by drs on Tue Dec 11 15:53:07 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This should be doable on this part. The USB stack nxpUSBlib has a mass storage class host example for this part but it only reads sectors. You would need to incorporate a FS (chanFS) on top of it to navigate the flash drive.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:50:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-USB-Bootloader-from-Usb-Memory-stick/m-p/521650#M4304</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:50:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPC17xx USB Bootloader from Usb Memory stick</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-USB-Bootloader-from-Usb-Memory-stick/m-p/521651#M4305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by RGB on Wed Dec 12 06:04:52 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you for the answer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But can I load all in bootloader? How can I do it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:50:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-USB-Bootloader-from-Usb-Memory-stick/m-p/521651#M4305</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:50:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPC17xx USB Bootloader from Usb Memory stick</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-USB-Bootloader-from-Usb-Memory-stick/m-p/521652#M4306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by drs on Thu Dec 20 11:11:56 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;No this is not possible. You can boot up and program your flash over UART0 using FlashMagic.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-USB-Bootloader-from-Usb-Memory-stick/m-p/521652#M4306</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:50:55Z</dc:date>
    </item>
  </channel>
</rss>