<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Can USB1 in high speed mode working with 12MHz system clock in LPC55S28 controller?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB1-in-high-speed-mode-working-with-12MHz-system-clock-in/m-p/1188072#M43016</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Jun Zhang,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for your reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So i have used and SDK example code "SDK_2.8.0_LPCXpresso55S28\boards\lpcxpresso55s28\usb_examples\usb_device_hid_generic\bm".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In that default system clock is 150MHz, and with LPC55S28 EVM kit USB1 as high speed works fine with above example code.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now if i change system clock to 12MHZ by using "BOARD_BootClockFRO12M" function in above example code, then USB1 as High-speed not working.&lt;/P&gt;&lt;P&gt;Note : with both usecase (12MHz and 150MHz system clock)16MHz crystal is connected to "XTAL32M" and USB1_PHY takes clock from that crystal.&lt;/P&gt;&lt;P&gt;Please find clock configuration image for 12MHz and 150MHz .&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rahul Shah&lt;/P&gt;</description>
    <pubDate>Tue, 24 Nov 2020 09:51:33 GMT</pubDate>
    <dc:creator>rahulshah</dc:creator>
    <dc:date>2020-11-24T09:51:33Z</dc:date>
    <item>
      <title>Can USB1 in high speed mode working with 12MHz system clock in LPC55S28 controller?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB1-in-high-speed-mode-working-with-12MHz-system-clock-in/m-p/1187020#M42979</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In our design it is required to use USB1 in high speed mode with 12MHz system clock.&lt;/P&gt;&lt;P&gt;So is USB1 in High-speed mode should work with 12MHz system clock? 12MHz system clock derived from FRO_12M.&lt;/P&gt;&lt;P&gt;Also in our design 12MHz crystal connected on XTAL32M for USB1-PHY clock.&lt;/P&gt;&lt;P&gt;So this solution should work or not? I have tested with different system clock as below and found following results.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;TABLE width="316"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="82"&gt;system clock&lt;/TD&gt;&lt;TD width="85"&gt;derived from&lt;/TD&gt;&lt;TD width="149"&gt;USB1 High speed status&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;12 MHz&lt;/TD&gt;&lt;TD&gt;FRO_12M&lt;/TD&gt;&lt;TD&gt;Not working&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;16 MHz&lt;/TD&gt;&lt;TD&gt;FRO_96M&lt;/TD&gt;&lt;TD&gt;Not working&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;19.2 MHz&lt;/TD&gt;&lt;TD&gt;FRO_96M&lt;/TD&gt;&lt;TD&gt;Not working&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;24 MHz&lt;/TD&gt;&lt;TD&gt;FRO_96M&lt;/TD&gt;&lt;TD&gt;Not working&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;32 MHz&lt;/TD&gt;&lt;TD&gt;FRO_96M&lt;/TD&gt;&lt;TD&gt;working&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;48 MHz&lt;/TD&gt;&lt;TD&gt;FRO_96M&lt;/TD&gt;&lt;TD&gt;working&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;96 MHz&lt;/TD&gt;&lt;TD&gt;FRO_96M&lt;/TD&gt;&lt;TD&gt;working&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;150MHz&lt;/TD&gt;&lt;TD&gt;PLL150M&lt;/TD&gt;&lt;TD&gt;working&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;50MHz&lt;/TD&gt;&lt;TD&gt;PLL150M&lt;/TD&gt;&lt;TD&gt;working&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;37.5MHz&lt;/TD&gt;&lt;TD&gt;PLL150M&lt;/TD&gt;&lt;TD&gt;working&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;30MHz&lt;/TD&gt;&lt;TD&gt;PLL150M&lt;/TD&gt;&lt;TD&gt;not working&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rahul Shah&lt;/P&gt;</description>
      <pubDate>Sun, 22 Nov 2020 12:03:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB1-in-high-speed-mode-working-with-12MHz-system-clock-in/m-p/1187020#M42979</guid>
      <dc:creator>rahulshah</dc:creator>
      <dc:date>2020-11-22T12:03:11Z</dc:date>
    </item>
    <item>
      <title>Re: Can USB1 in high speed mode working with 12MHz system clock in LPC55S28 controller?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB1-in-high-speed-mode-working-with-12MHz-system-clock-in/m-p/1188056#M43015</link>
      <description>&lt;P&gt;USB1 must work with external crystal osc. internal osc is not for USB1.&lt;/P&gt;
&lt;P&gt;see below:&lt;/P&gt;
&lt;P&gt;Initial configuration of the USB1_PHY:&lt;BR /&gt;• Clocks:&lt;BR /&gt;– The XO32M crystal oscillator and must be powered up and configured to one of the&lt;BR /&gt;supported USB1_PHY reference clock frequencies of 16 MHz, 19.2 MHz, 20 MHz,&lt;BR /&gt;24 MHz or 32 MHz. Set the ENABLE_USB_HS_CLK_OUT bit of the&lt;BR /&gt;XO32M_CTRL register to enable the XO32M clock output to the USB1_PHY. See&lt;BR /&gt;Section 11.5.5.&lt;BR /&gt;– Enable the 32k_osc clock to provide the 32 kHz clock to the USB1_PHY.&lt;BR /&gt;– Set USB1_PHY in AHBCLKCTRL2, to enable clock to the USB1_PHY’s APB&lt;BR /&gt;register interface&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 09:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB1-in-high-speed-mode-working-with-12MHz-system-clock-in/m-p/1188056#M43015</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-11-24T09:30:42Z</dc:date>
    </item>
    <item>
      <title>Re: Can USB1 in high speed mode working with 12MHz system clock in LPC55S28 controller?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB1-in-high-speed-mode-working-with-12MHz-system-clock-in/m-p/1188072#M43016</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Jun Zhang,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for your reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So i have used and SDK example code "SDK_2.8.0_LPCXpresso55S28\boards\lpcxpresso55s28\usb_examples\usb_device_hid_generic\bm".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In that default system clock is 150MHz, and with LPC55S28 EVM kit USB1 as high speed works fine with above example code.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now if i change system clock to 12MHZ by using "BOARD_BootClockFRO12M" function in above example code, then USB1 as High-speed not working.&lt;/P&gt;&lt;P&gt;Note : with both usecase (12MHz and 150MHz system clock)16MHz crystal is connected to "XTAL32M" and USB1_PHY takes clock from that crystal.&lt;/P&gt;&lt;P&gt;Please find clock configuration image for 12MHz and 150MHz .&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rahul Shah&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 09:51:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB1-in-high-speed-mode-working-with-12MHz-system-clock-in/m-p/1188072#M43016</guid>
      <dc:creator>rahulshah</dc:creator>
      <dc:date>2020-11-24T09:51:33Z</dc:date>
    </item>
  </channel>
</rss>