<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC54018 VDDA</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-VDDA/m-p/1184099#M42894</link>
    <description>&lt;P&gt;Looking at the LCP user manual (Page 1074) there is a line that says "The supply voltage VDD must be equal or lower than VDDA." I can find no similar statement in the datasheet; Table 12 (p. 79) gives the VDDA range as 2.7 - 3.6 V, making no mention of VDD.&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I was wondering what issue this may cause moving forward. I missed this line while doing the first prototype spin and have VDD running at 3.3v and VDDA running at 3.0v. Pushing forward with testing on this first spin I would like to know what issues I should expect to see with this configuration. So far validation has yet to present any issues.&lt;/DIV&gt;</description>
    <pubDate>Mon, 16 Nov 2020 23:08:46 GMT</pubDate>
    <dc:creator>smiller1</dc:creator>
    <dc:date>2020-11-16T23:08:46Z</dc:date>
    <item>
      <title>LPC54018 VDDA</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-VDDA/m-p/1184099#M42894</link>
      <description>&lt;P&gt;Looking at the LCP user manual (Page 1074) there is a line that says "The supply voltage VDD must be equal or lower than VDDA." I can find no similar statement in the datasheet; Table 12 (p. 79) gives the VDDA range as 2.7 - 3.6 V, making no mention of VDD.&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I was wondering what issue this may cause moving forward. I missed this line while doing the first prototype spin and have VDD running at 3.3v and VDDA running at 3.0v. Pushing forward with testing on this first spin I would like to know what issues I should expect to see with this configuration. So far validation has yet to present any issues.&lt;/DIV&gt;</description>
      <pubDate>Mon, 16 Nov 2020 23:08:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-VDDA/m-p/1184099#M42894</guid>
      <dc:creator>smiller1</dc:creator>
      <dc:date>2020-11-16T23:08:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 VDDA</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-VDDA/m-p/1185047#M42915</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please follow the UM statement of “The supply voltage VDD must be equal or lower than VDDA.”&lt;/P&gt;
&lt;P&gt;Exceeding of operating requirements may lead in device malfunction (reversible) or reduce life.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Wed, 18 Nov 2020 08:25:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-VDDA/m-p/1185047#M42915</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-11-18T08:25:28Z</dc:date>
    </item>
  </channel>
</rss>