<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックOutput bin file in mutli core application</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Output-bin-file-in-mutli-core-application/m-p/1176896#M42769</link>
    <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;We are designing a bootloader for customer product firmware update.&lt;BR /&gt;In LPC54114 mutli core application, there are M4 and M0 core and they have their own output bin file .&lt;BR /&gt;I would like to confirm that if I build slave project first then build master project ?&lt;BR /&gt;Is the output .bin file in debug folder of master project is already included both M4 and M0 output?&lt;BR /&gt;So I only need to flash the "lpcxpresso54114_mailbox_interrupt_mailbox_interrupt_cm4.bin" file in master project is enough for the dual core application. Please confirm.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Secondly, I have read AN12123.pdf for LPC541xx dual core starting guide, but I still have something confuse.&lt;BR /&gt;Is the code and data in M0 will finally stored in RAM1_90 but not in MFlash256 of master project after compiled?&lt;BR /&gt;The attached files Linker output report for my both master and slave projects.&lt;BR /&gt;Please kindly explain which Memory region the M0 core data and code will finally stored in M4.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Eric&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 03 Nov 2020 02:49:19 GMT</pubDate>
    <dc:creator>ericchan</dc:creator>
    <dc:date>2020-11-03T02:49:19Z</dc:date>
    <item>
      <title>Output bin file in mutli core application</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Output-bin-file-in-mutli-core-application/m-p/1176896#M42769</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;We are designing a bootloader for customer product firmware update.&lt;BR /&gt;In LPC54114 mutli core application, there are M4 and M0 core and they have their own output bin file .&lt;BR /&gt;I would like to confirm that if I build slave project first then build master project ?&lt;BR /&gt;Is the output .bin file in debug folder of master project is already included both M4 and M0 output?&lt;BR /&gt;So I only need to flash the "lpcxpresso54114_mailbox_interrupt_mailbox_interrupt_cm4.bin" file in master project is enough for the dual core application. Please confirm.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Secondly, I have read AN12123.pdf for LPC541xx dual core starting guide, but I still have something confuse.&lt;BR /&gt;Is the code and data in M0 will finally stored in RAM1_90 but not in MFlash256 of master project after compiled?&lt;BR /&gt;The attached files Linker output report for my both master and slave projects.&lt;BR /&gt;Please kindly explain which Memory region the M0 core data and code will finally stored in M4.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Eric&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Nov 2020 02:49:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Output-bin-file-in-mutli-core-application/m-p/1176896#M42769</guid>
      <dc:creator>ericchan</dc:creator>
      <dc:date>2020-11-03T02:49:19Z</dc:date>
    </item>
    <item>
      <title>Re: Output bin file in mutli core application</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Output-bin-file-in-mutli-core-application/m-p/1179192#M42797</link>
      <description>&lt;P&gt;HI&lt;/P&gt;
&lt;P&gt;For dual core project, we build slave project first then build master. Thus the slave generated image will be added to master during building master. That's to say, master image includes slave.&lt;/P&gt;
&lt;P&gt;Below is a master project setting that links of slave project:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1604643208412.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/129286i486F5C0D2D2948D6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1604643208412.png" alt="ZhangJennie_0-1604643208412.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ZhangJennie_0-1604643208412.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;When download master project, both master+slave images are downloaded.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Fri, 06 Nov 2020 06:14:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Output-bin-file-in-mutli-core-application/m-p/1179192#M42797</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-11-06T06:14:26Z</dc:date>
    </item>
  </channel>
</rss>