<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC55S69 PUF SDK Example</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-PUF-SDK-Example/m-p/1174039#M42717</link>
    <description>&lt;P&gt;Hi Ximena,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. After the PUF Enroll, the PUF must be power-cycled, and started by the PUF Start command. This is done with the sequence of PUF_Deinit and PUF_Init functions, or with the PUF_PowerCycle function. After that, you can use the PUF_Start function.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
    <pubDate>Tue, 27 Oct 2020 18:33:24 GMT</pubDate>
    <dc:creator>nxf58474</dc:creator>
    <dc:date>2020-10-27T18:33:24Z</dc:date>
    <item>
      <title>LPC55S69 PUF SDK Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-PUF-SDK-Example/m-p/1171853#M42676</link>
      <description>&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I am just beginning to work with PUFs and was looking at the SDK examples using PUF. I am working with the LPCXpresso55S69-EVK and MCUXpresso IDE. The example I am referring to is in driver_examples &amp;gt; puf.&lt;/P&gt;&lt;P&gt;I think the example wants to show all the different PUF functions and how they are used. But I stumbled upon the order of the functions, which is:&lt;BR /&gt;PUF_Init, PUF_Enroll, PUF_Deinit, PUF_Init, PUF_Start, etc.&lt;/P&gt;&lt;P&gt;Is there a particular reason why between PUF_Enroll and PUF_Start there is this additional PUF_Deinit/PUF_Init sequence? I would have guessed that one initialization at the beginning is enough and there is no need for a deinitialization followed by an initialization in between...&lt;/P&gt;&lt;P&gt;I have read the UM11126 and AN12324 and still do not understand why this is done in the example. Is it just to show the functionality of PUF_Deinit? Or is there a "deeper" reason behind it?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Ximena&lt;/P&gt;</description>
      <pubDate>Thu, 22 Oct 2020 13:08:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-PUF-SDK-Example/m-p/1171853#M42676</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2020-10-22T13:08:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 PUF SDK Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-PUF-SDK-Example/m-p/1174039#M42717</link>
      <description>&lt;P&gt;Hi Ximena,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. After the PUF Enroll, the PUF must be power-cycled, and started by the PUF Start command. This is done with the sequence of PUF_Deinit and PUF_Init functions, or with the PUF_PowerCycle function. After that, you can use the PUF_Start function.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 18:33:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-PUF-SDK-Example/m-p/1174039#M42717</guid>
      <dc:creator>nxf58474</dc:creator>
      <dc:date>2020-10-27T18:33:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 PUF SDK Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-PUF-SDK-Example/m-p/1178710#M42789</link>
      <description>&lt;P&gt;Hi Ricardo,&lt;/P&gt;&lt;P&gt;thanks for your explanation! It is much clearer now!&lt;/P&gt;&lt;P&gt;All the best&lt;BR /&gt;Ximena&lt;/P&gt;</description>
      <pubDate>Thu, 05 Nov 2020 10:22:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-PUF-SDK-Example/m-p/1178710#M42789</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2020-11-05T10:22:47Z</dc:date>
    </item>
  </channel>
</rss>