<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPCXpresso IDE: IOException during Debug of Sample Project</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170808#M42650</link>
    <description>&lt;P&gt;Hi converse,&lt;/P&gt;&lt;P&gt;thanks for your quick answer. Are you sure that this is the problem here? Could this be the reason that I cannot choose a core?&lt;/P&gt;&lt;P&gt;I wanted to use Windows as all the tutorials and side programs (like teraterm etc.) are for/with Windows. And I also worked with an eclipse-based IDE from TI (Code Composer Studio with an MSP430) on the VM, and it worked fine.&lt;/P&gt;&lt;P&gt;But ok, I guess it is worth a try to download it for Linux.&lt;/P&gt;</description>
    <pubDate>Wed, 21 Oct 2020 08:44:02 GMT</pubDate>
    <dc:creator>Anonymous</dc:creator>
    <dc:date>2020-10-21T08:44:02Z</dc:date>
    <item>
      <title>LPCXpresso IDE: IOException during Debug of Sample Project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170280#M42638</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I'm new to NXP microcontrollers and working with the LPCXpresso55S69-EVK. I am currently following the instructions on the "Get Started with the LPC55S69" &lt;A href="https://www.nxp.com/document/guide/get-started-with-the-lpc55s69-evk:GS-LPC55S69-EVK#title2.4" target="_blank" rel="noopener"&gt;site&lt;/A&gt;. My host system is Linux, but I am installing everything on a Windows VM with Oracle VM VirtualBox. There I have installed Windows 7 Ultimate.&lt;/P&gt;&lt;P&gt;So what I have done so far is everything from the videos:&lt;BR /&gt;1. Downloaded MCUXPRESSO SDK&lt;BR /&gt;2. Installed MCUXPRESSO IDE&lt;BR /&gt;3. Drag &amp;amp; Drop the SDK zip into the "Installed SDKs" windows&lt;BR /&gt;4. Installed LPCScrypt and updated the debug probe&lt;BR /&gt;5. Installed Tera Term as serial terminal&lt;BR /&gt;6. Chose the example project "Drivers &amp;gt; GPIO" like in the video&lt;BR /&gt;7. Built the project -&amp;gt; worked fine&lt;BR /&gt;8. Debug the project -&amp;gt; problem!&lt;/P&gt;&lt;P&gt;When I clicked on "Debug", I also got the first window "Probe Discovered" and clicked on "ok". But then I never saw the second window, where I could choose the core, and suddenly I got a lot of error messages (see below).&lt;/P&gt;&lt;P&gt;I tried plugging in and out the board, and restarting the IDE. But the error remains and I have no idea what the problem is.&lt;/P&gt;&lt;P&gt;Could anyone help/hint me please?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error Messages:&lt;/STRONG&gt;&lt;BR /&gt;1. Window: Target Discovery SWD Discovery&lt;BR /&gt;2. Window: MCUXpresso IDE: Exception (Error 1)&lt;BR /&gt;3. Window: Problem Occurred (Error 2)&lt;BR /&gt;4. Window: Error reported by Target (Error 3)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Message in Console:&lt;/STRONG&gt;&lt;BR /&gt;MCUXpresso IDE RedlinkMulti Driver v11.2 (Sep 22 2020 13:23:35 - crt_emu_cm_redlink build 19)&lt;BR /&gt;Found chip XML file in C:/Users/lea/Documents/MCUXpressoIDE_11.2.1_4149/workspace/lpcxpresso55s69_gpio_led_output/Debug\LPC55S69.xml&lt;BR /&gt;( 5) Remote configuration complete&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;Connecting to probe 1 core 0 (using server started externally) reports:&lt;BR /&gt;'Ee(42). Could not connect to core.'&lt;BR /&gt;Retrying...&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.&lt;BR /&gt;Failed on connect: Ee(42). Could not connect to core.&lt;BR /&gt;No connection to chip's debug port&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;EDIT:&lt;/STRONG&gt;&lt;BR /&gt;I don't know if this is relevant, but I saw, that the RedLink Server wants to use JTAG. but I thought it should use SWD. Or am I mixing something here?&lt;BR /&gt;This is the output:&lt;/P&gt;&lt;P&gt;[Started server]&lt;BR /&gt;[Connected on port 3025]&lt;BR /&gt;redlink&amp;gt; ProbeList&lt;BR /&gt;Index = 1&lt;BR /&gt;Manufacturer = NXP Semiconductors&lt;BR /&gt;Description = LPC-LINK2 CMSIS-DAP V5.361&lt;BR /&gt;Serial Number = ORA4CQFR&lt;BR /&gt;VID:PID = 1FC9:0090&lt;BR /&gt;Path = \\?\hid#vid_1fc9&amp;amp;pid_0090&amp;amp;mi_00#7&amp;amp;3a0fb07e&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;redlink&amp;gt; ProbeStatus&lt;BR /&gt;Index = 1&lt;BR /&gt;Manufacturer = NXP Semiconductors&lt;BR /&gt;Description = LPC-LINK2 CMSIS-DAP V5.361&lt;BR /&gt;Serial Number = ORA4CQFR&lt;BR /&gt;VID:PID = 1FC9:0090&lt;BR /&gt;Path = \\?\hid#vid_1fc9&amp;amp;pid_0090&amp;amp;mi_00#7&amp;amp;3a0fb07e&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;IsOpen = FALSE&lt;BR /&gt;WireInitialized = FALSE&lt;BR /&gt;WireProtocol = JTAG&lt;BR /&gt;CoresConfigured = FALSE&lt;BR /&gt;PacketSize = 1024&lt;BR /&gt;Reference Count = 0&lt;BR /&gt;HasSWV = FALSE&lt;BR /&gt;HasETM = FALSE&lt;BR /&gt;HasJTAG = TRUE&lt;BR /&gt;HasSWD = TRUE&lt;BR /&gt;Probe Type = CMSIS-DAP&lt;BR /&gt;Probe Reference Count = 0&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 11:23:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170280#M42638</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2020-10-20T11:23:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso IDE: IOException during Debug of Sample Project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170354#M42639</link>
      <description>&lt;P&gt;VirtualBox is a decent&amp;nbsp;VM but it’s USB emulation is poor. Basically it can’t cope with the high speed required of debugging. &amp;nbsp;As you are running in Linux, why not just use the Linux version of MCUXpresso?&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 12:42:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170354#M42639</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-10-20T12:42:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso IDE: IOException during Debug of Sample Project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170626#M42648</link>
      <description>&lt;P&gt;Hello &lt;SPAN class="UserName lia-user-name lia-user-rank-Fresh-Out-Contributor lia-component-message-view-widget-author-username"&gt;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" style="color: #333f48;" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179312" target="_self"&gt;&lt;SPAN class=""&gt;Ximena&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can directly download and install Linux version MCUXpresso IDE:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://freescaleesd.flexnetoperations.com/337170/687/17360687/mcuxpressoide-11.2.1_4149.x86_64.deb.bin?ftpRequestID=8078628327&amp;amp;server=freescaleesd.flexnetoperations.com&amp;amp;dtm=DTM20201021032717OTA0ODIyMjYz&amp;amp;authparam=1603276037_9e6e0ef022b79fbe760b04ecbe046348&amp;amp;ext=.bin" target="_blank"&gt;https://freescaleesd.flexnetoperations.com/337170/687/17360687/mcuxpressoide-11.2.1_4149.x86_64.deb.bin?ftpRequestID=8078628327&amp;amp;server=freescaleesd.flexnetoperations.com&amp;amp;dtm=DTM20201021032717OTA0ODIyMjYz&amp;amp;authparam=1603276037_9e6e0ef022b79fbe760b04ecbe046348&amp;amp;ext=.bin&lt;/A&gt; &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 02:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170626#M42648</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2020-10-21T02:33:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso IDE: IOException during Debug of Sample Project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170808#M42650</link>
      <description>&lt;P&gt;Hi converse,&lt;/P&gt;&lt;P&gt;thanks for your quick answer. Are you sure that this is the problem here? Could this be the reason that I cannot choose a core?&lt;/P&gt;&lt;P&gt;I wanted to use Windows as all the tutorials and side programs (like teraterm etc.) are for/with Windows. And I also worked with an eclipse-based IDE from TI (Code Composer Studio with an MSP430) on the VM, and it worked fine.&lt;/P&gt;&lt;P&gt;But ok, I guess it is worth a try to download it for Linux.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 08:44:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170808#M42650</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2020-10-21T08:44:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso IDE: IOException during Debug of Sample Project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170834#M42651</link>
      <description>&lt;P&gt;Hi Alice_Yang,&lt;/P&gt;&lt;P&gt;thanks for the link! When installing it on Linux, do I also have to do step 2.4 updating the debug probe firmware via LPCScrypt? Somehwere in video he said that some points are not necessary when using Linux.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 08:01:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170834#M42651</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2020-10-21T08:01:15Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso IDE: IOException during Debug of Sample Project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170867#M42653</link>
      <description>&lt;P&gt;It is normally a good idea - it makes sure you have the latest version of the Debug Probe firmware.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 08:46:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170867#M42653</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-10-21T08:46:17Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso IDE: IOException during Debug of Sample Project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170870#M42654</link>
      <description>&lt;P&gt;Commercial VM's work well in all scenarios. VirtualBox works well - except for the USB.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 08:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170870#M42654</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-10-21T08:50:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso IDE: IOException during Debug of Sample Project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170874#M42655</link>
      <description>&lt;P&gt;Ok, updated the debug probe firmware with LPCScrypt for Linux and tried the example gpio led program again (on Linux) and it is working fine!!&lt;/P&gt;&lt;P&gt;So it seems that the VM really was the problem - like you suggested. I was just confused as it worked so well with the MSP430 and CCS. But ok, I guess every MCU is different &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;Happy that it works now and thank you very much for your help!&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 08:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso-IDE-IOException-during-Debug-of-Sample-Project/m-p/1170874#M42655</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2020-10-21T08:56:33Z</dc:date>
    </item>
  </channel>
</rss>