<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC824 is not waking up from power-down with pin interrupt</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1170229#M42636</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;But I need the WKT. The microcontroller shall wake up from pin change or every x seconds if there is no pin interrupt. And as already said it works both well, but not at the same time. If I disable the WKT, the pin wakeup works fine. If I enable the WKT, the timer wakeup works fine but the pin wakeup does not work anymore.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
    <pubDate>Tue, 20 Oct 2020 09:01:26 GMT</pubDate>
    <dc:creator>robin_maeder</dc:creator>
    <dc:date>2020-10-20T09:01:26Z</dc:date>
    <item>
      <title>LPC824 is not waking up from power-down with pin interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1165850#M42530</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am trying to wake up the LPC824 from Deep-sleep or Power-down with an external pin but I can not get it working. I tried it according to &lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Power-Down-PIN-Interrupt-wakeup-issue/m-p/1165739#M42528" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Power-Down-PIN-Interrupt-wakeup-issue/m-p/1165739#M42528&lt;/A&gt;. I tried it according to the example&amp;nbsp;lpcxpresso824max_power_mode_switch_lpc from SDK. But it does not work either way.&lt;/P&gt;&lt;P&gt;1. Is it possible to use PINT for waking up the LPC824? In the following post they say that&amp;nbsp;pin&amp;nbsp;&lt;SPAN&gt;interrupt is incapable of waking up the MCU from the Deep-sleep or Power-down on LPC11xx?&amp;nbsp;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/How-to-wake-up-the-system-from-deep-sleep-mode-with-pin/m-p/745364/highlight/true" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/How-to-wake-up-the-system-from-deep-sleep-mode-wit...&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. Is there another way or example for waking up with pin interrupt?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you and best regards.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2020 06:50:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1165850#M42530</guid>
      <dc:creator>robin_maeder</dc:creator>
      <dc:date>2020-10-12T06:50:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 is not waking up from power-down with pin interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1166624#M42543</link>
      <description>&lt;P&gt;Hello Robin,&lt;/P&gt;
&lt;P&gt;What about the phenomenon when you press wake up pin?&lt;/P&gt;
&lt;P&gt;How about run project alone without debugger?&lt;/P&gt;
&lt;P&gt;Also I will help to test on my side.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 09:03:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1166624#M42543</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2020-10-13T09:03:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 is not waking up from power-down with pin interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1166634#M42544</link>
      <description>&lt;P&gt;Hi Alice&lt;/P&gt;&lt;P&gt;Thank you for your answer. I will try it with the wake-up pin. There is no debugger connected during testing.&lt;/P&gt;&lt;P&gt;Can you say if the wake-up shoud work with PINT interrupt or not?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 09:15:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1166634#M42544</guid>
      <dc:creator>robin_maeder</dc:creator>
      <dc:date>2020-10-13T09:15:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 is not waking up from power-down with pin interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1167205#M42554</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;"&lt;SPAN style="font-family: inherit;"&gt;Can you say if the wake-up shoud work with PINT interrupt or not?"&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-family: inherit;"&gt;-&amp;gt; Yes, it should be work.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-family: inherit;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-family: inherit;"&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2020 06:39:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1167205#M42554</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2020-10-14T06:39:09Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 is not waking up from power-down with pin interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1169493#M42619</link>
      <description>&lt;P&gt;Hello Alice&lt;/P&gt;&lt;P&gt;I got it working with the PINT. The problems were that I called the power down command from inside a PINT callback function and "EnableDeepSleepIRQ(PIN_INTx_IRQn)" was missing.&lt;/P&gt;&lt;P&gt;But now I have another problem. I want to wake up the controller from either the PINT interrupt or the WKT timer. WKT alone works finde, PINT alone works fine. But as soon as I start the WKT timer before going into deep sleep mode, the PINT wakeup does not work anymore.&lt;/P&gt;&lt;P&gt;Any ideas about that &lt;SPAN&gt;phenomenon?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Oct 2020 08:44:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1169493#M42619</guid>
      <dc:creator>robin_maeder</dc:creator>
      <dc:date>2020-10-19T08:44:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 is not waking up from power-down with pin interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1170226#M42635</link>
      <description>&lt;P&gt;Hello&lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt; &lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" style="color: #333f48;" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/159025" target="_self"&gt;&lt;SPAN class=""&gt;robin_maeder,&lt;/SPAN&gt;&lt;/A&gt; &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt;&lt;SPAN class=""&gt;I think you can disable the WKT timer in your project, check whether the PIN interrupt can work well.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt;&lt;SPAN class=""&gt;Regards,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt;&lt;SPAN class=""&gt;Alice&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;DIV class="lia-message-author-with-avatar"&gt;
&lt;DIV class="lia-message-author-rank lia-component-author-rank lia-component-message-view-widget-author-rank"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Tue, 20 Oct 2020 08:57:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1170226#M42635</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2020-10-20T08:57:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 is not waking up from power-down with pin interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1170229#M42636</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;But I need the WKT. The microcontroller shall wake up from pin change or every x seconds if there is no pin interrupt. And as already said it works both well, but not at the same time. If I disable the WKT, the pin wakeup works fine. If I enable the WKT, the timer wakeup works fine but the pin wakeup does not work anymore.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 09:01:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1170229#M42636</guid>
      <dc:creator>robin_maeder</dc:creator>
      <dc:date>2020-10-20T09:01:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 is not waking up from power-down with pin interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1170735#M42649</link>
      <description>&lt;P&gt;Hello&lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt; &lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" style="color: #333f48;" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/159025" target="_self"&gt;&lt;SPAN class=""&gt;robin_maeder,&lt;/SPAN&gt;&lt;/A&gt; &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Please share your project that I can help to test and check on my side.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 06:11:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1170735#M42649</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2020-10-21T06:11:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 is not waking up from power-down with pin interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1171172#M42662</link>
      <description>&lt;P&gt;I found the problem. Before going into power down I disabled the interrupt callback. After that I had to enable DeepSleepIRQ again.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 17:19:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1171172#M42662</guid>
      <dc:creator>robin_maeder</dc:creator>
      <dc:date>2020-10-21T17:19:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 is not waking up from power-down with pin interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1171667#M42673</link>
      <description>&lt;P&gt;OK.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Oct 2020 08:31:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-is-not-waking-up-from-power-down-with-pin-interrupt/m-p/1171667#M42673</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2020-10-22T08:31:20Z</dc:date>
    </item>
  </channel>
</rss>