<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックSPIFI-NXP-MICROCONTROLLERS: LPC SPIFI Peripheral - Cypress S25FL064LABNFI013</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-NXP-MICROCONTROLLERS-LPC-SPIFI-Peripheral-Cypress/m-p/1162873#M42463</link>
    <description>&lt;P&gt;Hi, I am using the LPC SPIFI Peripheral Library:&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;MCUXpressoIDE_11.2.0_4120\ide\Examples\Flashdrivers\NXP\LPC5460x\LPC5460x_lpcspifilib_driver.zip\LPC5460x_SPIFIdriver_Generic\lpcspifilib&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Will there be any updates to this library to add new devices?&lt;/P&gt;&lt;P&gt;Will NXP add the SPIF device "&lt;FONT&gt;Cypress S25FL064LABNFI013" to this library?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;If yes, when will this update be available?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Many Thanks&lt;/P&gt;&lt;P&gt;Dani&lt;/P&gt;</description>
    <pubDate>Mon, 05 Oct 2020 10:30:18 GMT</pubDate>
    <dc:creator>danielgull</dc:creator>
    <dc:date>2020-10-05T10:30:18Z</dc:date>
    <item>
      <title>SPIFI-NXP-MICROCONTROLLERS: LPC SPIFI Peripheral - Cypress S25FL064LABNFI013</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-NXP-MICROCONTROLLERS-LPC-SPIFI-Peripheral-Cypress/m-p/1162873#M42463</link>
      <description>&lt;P&gt;Hi, I am using the LPC SPIFI Peripheral Library:&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;MCUXpressoIDE_11.2.0_4120\ide\Examples\Flashdrivers\NXP\LPC5460x\LPC5460x_lpcspifilib_driver.zip\LPC5460x_SPIFIdriver_Generic\lpcspifilib&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Will there be any updates to this library to add new devices?&lt;/P&gt;&lt;P&gt;Will NXP add the SPIF device "&lt;FONT&gt;Cypress S25FL064LABNFI013" to this library?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;If yes, when will this update be available?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Many Thanks&lt;/P&gt;&lt;P&gt;Dani&lt;/P&gt;</description>
      <pubDate>Mon, 05 Oct 2020 10:30:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-NXP-MICROCONTROLLERS-LPC-SPIFI-Peripheral-Cypress/m-p/1162873#M42463</guid>
      <dc:creator>danielgull</dc:creator>
      <dc:date>2020-10-05T10:30:18Z</dc:date>
    </item>
    <item>
      <title>Re: SPIFI-NXP-MICROCONTROLLERS: LPC SPIFI Peripheral - Cypress S25FL064LABNFI013</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-NXP-MICROCONTROLLERS-LPC-SPIFI-Peripheral-Cypress/m-p/1165332#M42518</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/165257"&gt;@danielgull&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Until now there's is no news about this device being added to the library but you can modify the library add the support for new devices. In the following presentation, there is some consideration to modify the SPIFI library.&lt;/P&gt;
&lt;P&gt;It looks like this memory support the same serial command structure as the one already added to the library (S25FL-P), I will suggest looking at the commands used by this memory and also look in the SPIFI examples found in the SDK.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Fri, 09 Oct 2020 16:28:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-NXP-MICROCONTROLLERS-LPC-SPIFI-Peripheral-Cypress/m-p/1165332#M42518</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-10-09T16:28:36Z</dc:date>
    </item>
  </channel>
</rss>