<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Problem with LPCXpresso55S69 Dev Board and blhost</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LPCXpresso55S69-Dev-Board-and-blhost/m-p/1162273#M42454</link>
    <description>&lt;P&gt;In case others are struggling with this or a similar issue, I was able to resolve it by looking at a Ubuntu system that had a working MCUXpresso IDE installed. The breakthrough moment came when I found the driver that was being used by the /dev/ttyACM0 device that was being created when I plugged the board in (this device was not being created on my Gentoo system). The board uses the CDC ACM kernel module. After I reconfigured the kernel with this module set to compile, I plugged the board in and the /dev/ttyACM0 device was created on the Gentoo system. Rather than issuing the command:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;blhost -d -u 0x1fc9,0x0090 get-property 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I issued the command:&lt;/P&gt;&lt;P&gt;blhost -n -d -p /dev/ttyACM0 -- get-property 1&lt;/P&gt;&lt;P&gt;This worked. I was also able to throw together a Gentoo EBuild for the MCUXpresso IDE and now I have the IDE installed and working.&lt;/P&gt;</description>
    <pubDate>Fri, 02 Oct 2020 13:50:29 GMT</pubDate>
    <dc:creator>tim_t_fake</dc:creator>
    <dc:date>2020-10-02T13:50:29Z</dc:date>
    <item>
      <title>Problem with LPCXpresso55S69 Dev Board and blhost</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LPCXpresso55S69-Dev-Board-and-blhost/m-p/1161895#M42446</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to start development with the LPCXpresso55S69 development board. I am running the Gentoo Linux Distro. I have tested the board in Windows with the MCUXpresso IDE and everything works. I would like to use VIM as my code editor and I would like to use the blhost utility to flash to the chip. I am trying to send some basic commands to the chip to see if I can get a response. Below is one such command and the result:&lt;/P&gt;&lt;P&gt;----------------------------------------------------------&lt;/P&gt;&lt;P&gt;Command:&lt;/P&gt;&lt;P&gt;blhost -d -u 0x1fc9,0x0090 get-property 1&lt;/P&gt;&lt;P&gt;Result:&lt;/P&gt;&lt;P&gt;Inject command 'get-property'&lt;BR /&gt;[01 00 0c 00 07 00 00 02 01 00 00 00 00 00 00 00]&lt;BR /&gt;usb hid write, time left = 5000&lt;BR /&gt;&amp;lt;01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00&amp;gt;&lt;BR /&gt;usbhid: received unexpected report=1&lt;BR /&gt;sendCommandGetResponse.readPacket error 1.&lt;BR /&gt;processResponse: null packet&lt;BR /&gt;- took 0.001 seconds&lt;BR /&gt;Response status = 10004 (0x2714) No response packet from target device&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Any help that anyone could give me to get this working would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Oct 2020 17:44:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LPCXpresso55S69-Dev-Board-and-blhost/m-p/1161895#M42446</guid>
      <dc:creator>tim_t_fake</dc:creator>
      <dc:date>2020-10-01T17:44:06Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with LPCXpresso55S69 Dev Board and blhost</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LPCXpresso55S69-Dev-Board-and-blhost/m-p/1162273#M42454</link>
      <description>&lt;P&gt;In case others are struggling with this or a similar issue, I was able to resolve it by looking at a Ubuntu system that had a working MCUXpresso IDE installed. The breakthrough moment came when I found the driver that was being used by the /dev/ttyACM0 device that was being created when I plugged the board in (this device was not being created on my Gentoo system). The board uses the CDC ACM kernel module. After I reconfigured the kernel with this module set to compile, I plugged the board in and the /dev/ttyACM0 device was created on the Gentoo system. Rather than issuing the command:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;blhost -d -u 0x1fc9,0x0090 get-property 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I issued the command:&lt;/P&gt;&lt;P&gt;blhost -n -d -p /dev/ttyACM0 -- get-property 1&lt;/P&gt;&lt;P&gt;This worked. I was also able to throw together a Gentoo EBuild for the MCUXpresso IDE and now I have the IDE installed and working.&lt;/P&gt;</description>
      <pubDate>Fri, 02 Oct 2020 13:50:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LPCXpresso55S69-Dev-Board-and-blhost/m-p/1162273#M42454</guid>
      <dc:creator>tim_t_fake</dc:creator>
      <dc:date>2020-10-02T13:50:29Z</dc:date>
    </item>
  </channel>
</rss>