<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPCScrypt not working in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1161483#M42439</link>
    <description>&lt;P&gt;Hope you are well. I tried the installation fresh and I didn't have any problems programming with JLINK.&lt;/P&gt;
&lt;P&gt;I am using ubuntu 16.04 64 bit OS.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I used the &lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2-1-1:LPCSCRYPT" target="_self"&gt;standalone&lt;/A&gt; installation for linux and did the following:&lt;/P&gt;
&lt;P&gt;sudo chmod +x&amp;nbsp;lpcscrypt-2.1.1_15.x86_64.deb.bin&lt;/P&gt;
&lt;P&gt;sudo ./lpcscrypt-2.1.1_15.x86_64.deb.bin&lt;/P&gt;
&lt;P&gt;Then in the script folder I called the script needed and ran successfully.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Sabina&lt;/P&gt;</description>
    <pubDate>Wed, 30 Sep 2020 18:16:42 GMT</pubDate>
    <dc:creator>Sabina_Bruce</dc:creator>
    <dc:date>2020-09-30T18:16:42Z</dc:date>
    <item>
      <title>LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1133074#M42113</link>
      <description>&lt;P&gt;I'm trying to use program_JLINK to install JLink on my eval board for the LPC55S69 on Ubuntu 19.04. When I run the script, it hangs in the loop where it does lpcscrypt print 1234.&lt;/P&gt;&lt;P&gt;When I run lpcscrypt print 1234 by hand, it hangs up for a while, and then exits with the following message:&lt;/P&gt;&lt;P&gt;/usr/local/lpcscrypt/bin/lpcscrypt print&lt;BR /&gt;Error opening /dev/ttyUSB0: Resource temporarily unavailable&lt;BR /&gt;(Sometimes ISP reset, or erasing the flash, can help...)&lt;BR /&gt;Previous error(s) stops further processing&lt;BR /&gt;Error: &amp;lt;Command line&amp;gt;:0: Resource temporarily unavailable&lt;BR /&gt;Script cmd: batchmode 1&lt;BR /&gt;Last target cmd: =print 1940686103&lt;BR /&gt;Terminated with errors&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Roger Strassburg&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 12:25:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1133074#M42113</guid>
      <dc:creator>r_strassburg</dc:creator>
      <dc:date>2020-09-01T12:25:07Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1133221#M42114</link>
      <description>&lt;P&gt;According to the information for LPCScrypt:&lt;/P&gt;&lt;P&gt;LPCScrypt is a command-line based, fast flash, EEPROM, OTP and security programming tool for LPC1800 and LPC4300 series microcontrollers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Having said that, have you checked the permissions on /dev/ttyUSB0 (or any other ports with similar names)&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 16:40:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1133221#M42114</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-09-01T16:40:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1133258#M42116</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The permissions should be ok:&lt;/P&gt;&lt;P&gt;crw-rw-rw- 1 root dialout 188, 0 Sep 1 14:08 /dev/ttyUSB0&lt;/P&gt;&lt;P&gt;Also, I ran it under root, so there shouldn't be an issue with permissions.&lt;/P&gt;&lt;P&gt;Is there a different utility I should be using for the LPC55S69?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 17:37:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1133258#M42116</guid>
      <dc:creator>r_strassburg</dc:creator>
      <dc:date>2020-09-01T17:37:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1133289#M42117</link>
      <description>&lt;P&gt;Sorry, I see you are programming the onboard lpc-link2 whic is supported.&lt;/P&gt;&lt;P&gt;So, does the provided script work to program the firmware image?&lt;/P&gt;&lt;P&gt;sorry, no other ideas.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 18:27:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1133289#M42117</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-09-01T18:27:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1134168#M42126</link>
      <description>&lt;P&gt;No. That's why I asked for help.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2020 11:38:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1134168#M42126</guid>
      <dc:creator>r_strassburg</dc:creator>
      <dc:date>2020-09-02T11:38:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1134325#M42129</link>
      <description>&lt;P&gt;Hello Roger,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please confirm if you are experiencing this issue only on Ubuntu? Are you able to run the script successfully on windows?&lt;/P&gt;
&lt;P&gt;What version of the LPCScrypt are you using?&lt;/P&gt;
&lt;P&gt;Also could you please try the steps in the last reply of the following post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LCPScrypt-1-8-2-not-working-on-ubuntu-16-04/m-p/701079" target="_self"&gt;LPCScrypt not working on Ubuntu&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Let me know your results.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Sabina&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2020 14:14:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1134325#M42129</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-09-02T14:14:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1149844#M42157</link>
      <description>&lt;P&gt;Hi Sabina,&lt;/P&gt;&lt;P&gt;Thanks. I hope you're doing well, as well.&lt;/P&gt;&lt;P&gt;I've only tried this on Ubuntu, as I don't really have a Windows system to run it on. But a colleague of mine has been successfully running on Windows for some time.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Roger&lt;/P&gt;</description>
      <pubDate>Mon, 07 Sep 2020 18:03:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1149844#M42157</guid>
      <dc:creator>r_strassburg</dc:creator>
      <dc:date>2020-09-07T18:03:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1151624#M42185</link>
      <description>&lt;P&gt;Do the steps from the previous post, result positive for you?&lt;/P&gt;
&lt;P&gt;"1. Run "./program_JLINK" from the script directory as described. It will hang. This is the main issue.&lt;/P&gt;
&lt;P&gt;2. Use CTRL+C to break and return control back to the console.&lt;/P&gt;
&lt;P&gt;3. Run "./lpcscrypt print 0x1234" from the bin directory&lt;/P&gt;
&lt;P&gt;4. Once again, run "./program_JLINK" from the script directory. It will not hang this time and proceed to completion.&lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 14:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1151624#M42185</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-09-10T14:41:10Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1154332#M42265</link>
      <description>&lt;P&gt;Hi Sabina,&lt;/P&gt;&lt;P&gt;The suggested workaround didn't work for me. The USB&lt;/P&gt;</description>
      <pubDate>Wed, 16 Sep 2020 18:57:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1154332#M42265</guid>
      <dc:creator>r_strassburg</dc:creator>
      <dc:date>2020-09-16T18:57:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1154334#M42266</link>
      <description>&lt;P&gt;Thanks for the suggestion. I tried this but it didn't work for me. The USB device it's looking for is there, though:&lt;/P&gt;&lt;P&gt;Bus 001 Device 064: ID 1fc9:000c NXP Semiconductors&lt;/P&gt;&lt;P&gt;Roger&lt;/P&gt;</description>
      <pubDate>Wed, 16 Sep 2020 18:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1154334#M42266</guid>
      <dc:creator>r_strassburg</dc:creator>
      <dc:date>2020-09-16T18:58:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1155076#M42275</link>
      <description>&lt;P&gt;Could you please provide the version of the LPCScrypt that you are using.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Sabina&lt;/P&gt;</description>
      <pubDate>Thu, 17 Sep 2020 21:42:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1155076#M42275</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-09-17T21:42:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1159314#M42398</link>
      <description>&lt;P&gt;2.1.1_15&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 11:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1159314#M42398</guid>
      <dc:creator>r_strassburg</dc:creator>
      <dc:date>2020-09-25T11:24:44Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1161483#M42439</link>
      <description>&lt;P&gt;Hope you are well. I tried the installation fresh and I didn't have any problems programming with JLINK.&lt;/P&gt;
&lt;P&gt;I am using ubuntu 16.04 64 bit OS.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I used the &lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2-1-1:LPCSCRYPT" target="_self"&gt;standalone&lt;/A&gt; installation for linux and did the following:&lt;/P&gt;
&lt;P&gt;sudo chmod +x&amp;nbsp;lpcscrypt-2.1.1_15.x86_64.deb.bin&lt;/P&gt;
&lt;P&gt;sudo ./lpcscrypt-2.1.1_15.x86_64.deb.bin&lt;/P&gt;
&lt;P&gt;Then in the script folder I called the script needed and ran successfully.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Sabina&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2020 18:16:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1161483#M42439</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-09-30T18:16:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1183366#M42881</link>
      <description>&lt;P&gt;I'm using lpcscrypt 2.1.1 on Windows 10.&amp;nbsp; What are the chances that this error is caused by anti-malware such as Sophos?&amp;nbsp; We're not sure, but we started observing this Q3 or Q4 of 2020.&amp;nbsp; As of right now, no one can get lpcscrypt to work on windows at our facility where it worked perfectly before.&amp;nbsp; Same hardware, nothing else has changed.&amp;nbsp; It is able to boot the device, but no commands work after that.&amp;nbsp; The driver also says this: "Device USB\VID_1FC9&amp;amp;PID_0083\NXP-77 requires further installation."&lt;/P&gt;</description>
      <pubDate>Sat, 14 Nov 2020 06:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1183366#M42881</guid>
      <dc:creator>brich</dc:creator>
      <dc:date>2020-11-14T06:05:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1183370#M42882</link>
      <description>&lt;P&gt;“Nothing changed” - what about Windows updates?&lt;/P&gt;</description>
      <pubDate>Sat, 14 Nov 2020 08:33:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1183370#M42882</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-11-14T08:33:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1183394#M42883</link>
      <description>&lt;P&gt;Yes, Windows updates have been performed.&amp;nbsp; That was going to be my next question.&lt;/P&gt;</description>
      <pubDate>Sat, 14 Nov 2020 23:35:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1183394#M42883</guid>
      <dc:creator>brich</dc:creator>
      <dc:date>2020-11-14T23:35:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPCScrypt not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1527965#M50266</link>
      <description>&lt;P&gt;Any updates on this thread? I just got a similar issue with the latest version of LPCScrypt 2.1.2 on 64-bit Ubuntu 18.04.6 LTS. The LPCScrypt user guide specifically mentions:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;STRONG&gt;Note&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCScrypt for Linux is a 64-bit application, so it will not run on 32-bit systems.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It is supported and tested only on the Linux distribution Ubuntu 16.04 LTS and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;18.04 LTS.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I am using a fresh LPCXpresso54102 board with JP5 installed. This configuration allows me to use program_JLINK or program_CMSIS without the "Resource temporarily unavailable" error message. When I reboot with the DFULink jumper open to flash the target LPC54102 instead of the embedded link2 programmer, the serial port shows up on &lt;STRONG&gt;lsusb&lt;/STRONG&gt; and serializes as &lt;STRONG&gt;/dev/ttyACM0&lt;/STRONG&gt;, but running &lt;STRONG&gt;lpcscrypt print&lt;/STRONG&gt; manually, throws the "Resource temporarily unavailable" error. This is true regardless of the on-board LPC54102 MCU being in ISP mode or not. I've attached my terminal commands with their outputs.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Sep 2022 08:14:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCScrypt-not-working/m-p/1527965#M50266</guid>
      <dc:creator>jlrojas93</dc:creator>
      <dc:date>2022-09-26T08:14:15Z</dc:date>
    </item>
  </channel>
</rss>