<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPCXpresso54628 not found by IDE</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-not-found-by-IDE/m-p/1161337#M42436</link>
    <description>&lt;P&gt;Did you connect to J8 and check the jumpers? Read&amp;nbsp;UM11035 section 3.2.1 for information&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 30 Sep 2020 12:46:57 GMT</pubDate>
    <dc:creator>converse</dc:creator>
    <dc:date>2020-09-30T12:46:57Z</dc:date>
    <item>
      <title>LPCXpresso54628 not found by IDE</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-not-found-by-IDE/m-p/1161258#M42434</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I have an OM13098/LPCXpresso54628 board.&lt;BR /&gt;I downloaded and installed the MCUXpresso IDE and the corresponding SDK (I'm on Windows 10, but have also tried this on Linux with the same reslut), but when installation is done and I try out any of the example projects (by running 'debug') I get the error message&amp;nbsp;&lt;/P&gt;&lt;P&gt;Connect to target LPC54628J512&lt;/P&gt;&lt;P&gt;No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There doesn't seem to be any serial usb-device showing up anywhere.&lt;/P&gt;&lt;P&gt;Is there any hard reset or something else I could try?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Anders&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2020 10:26:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-not-found-by-IDE/m-p/1161258#M42434</guid>
      <dc:creator>agenell</dc:creator>
      <dc:date>2020-09-30T10:26:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso54628 not found by IDE</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-not-found-by-IDE/m-p/1161337#M42436</link>
      <description>&lt;P&gt;Did you connect to J8 and check the jumpers? Read&amp;nbsp;UM11035 section 3.2.1 for information&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2020 12:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-not-found-by-IDE/m-p/1161337#M42436</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-09-30T12:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso54628 not found by IDE</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-not-found-by-IDE/m-p/1162033#M42450</link>
      <description>&lt;P&gt;It's a good idea to check the jumpers settings as Converse mentioned.&lt;/P&gt;
&lt;P&gt;Additionally, from the error message you are seeing it would appear as if the debug firmware was either erased or corrupted. You can flash this firmware easily using the LPCScrypt tool (available in the link below).&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2-1-1:LPCSCRYPT?tab=Design_Tools_Tab" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2-1-1:LPCSCRYPT?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Once installed in your host computer, please follow these steps:&lt;/P&gt;
&lt;P&gt;Force DFU boot on your board. This can be achieved by placing a jumper in JP5.&lt;/P&gt;
&lt;P&gt;Connect the USB Debug port to the computer.&lt;/P&gt;
&lt;P&gt;Open a terminal and run:&lt;BR /&gt;&amp;lt;LPCScrypt Install Dir&amp;gt;\scripts\program_JLINK &lt;BR /&gt;Or&lt;BR /&gt;&amp;lt;LPCScrypt Install Dir&amp;gt;\scripts\program_CMSIS &lt;BR /&gt;Depending on whether you wish to use JLINK or CMSIS. (Both work with MCUXpresso SDK)&lt;/P&gt;
&lt;P&gt;(C:\nxp\LPCScrypt_2.0.0_831\ is the default installation path of the latest version of LPCScrypt for Windows 10)&lt;/P&gt;
&lt;P&gt;The LPCScrypt tool will then connect to the board and program the firmware. Once it’s done quit the tool using CTRL+C.&lt;/P&gt;
&lt;P&gt;You may then disconnect the board, take out the JP5 jumper (optionally), and try debugging again.&lt;/P&gt;
&lt;P&gt;I hope that this information helps.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Thu, 01 Oct 2020 20:20:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-not-found-by-IDE/m-p/1162033#M42450</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-10-01T20:20:27Z</dc:date>
    </item>
  </channel>
</rss>